Skip to main content
SSaiy.1
Associate III
February 13, 2023
Solved

STM32 L412 Timer interrupt not working

I am using STM32L412 microcontroller and doing baremetal programming for timer interrupt. I am using Timer 6 and base clock of 4MHZ is used as HCLK. However my interrupt is not firing below mentioning my code. count variable is also not updating

int main(void)

{

LedConfig();

StartTimer6();

  /* Loop forever */

while(1)

{

count=1;

}

}

void LedConfig(void)

{

/*Enable Clock for Port B. */

RCC->AHB2ENR |= (1U<<1);

/*Configure GPIOB_13 as general purpose output*/

GPIOB->MODER |= (1U<<26);

GPIOB->MODER &= ~(1U<<27);

}

void StartTimer6(void)

{

RCC->APB1ENR1 |= (1U<<4);

TIM6->PSC = 1000;

TIM6->ARR = 4000;

TIM6->EGR |= (1U<<0);

TIM6->DIER |= (1U<<0);

TIM6->CR1 |= (1U<<0);

NVIC_EnableIRQ(TIM6_IRQn);

}

void TIM6_IRQHandler(void)

{

if(TIM6->SR & (1U<<0))

{

GPIOB->ODR ^= (1U<<13);

TIM6->SR &= ~(1U<<0);

}

}

    This topic has been closed for replies.
    SSaiy.1
    SSaiy.1Best answer
    Associate III
    February 14, 2023

    Thanks @KnarfB as you said IRQ handler was different the actual one is TIM6_DACUNDER_IRQHandler. After I changed the handler name the code started working

    14 replies

    KnarfB
    Super User
    February 13, 2023

    no code, no description, no answer...

    SSaiy.1
    SSaiy.1Author
    Associate III
    February 13, 2023

    @KnarfB​ Sorry, I was entering the details.

    KnarfB
    Super User
    February 13, 2023

    And CNT register updating?

    Ref.man,. talks about delay after enabling peripheral clocks, maybe

    RCC->APB1ENR1 |= RCC_APB1ENR1_TIM6EN; // set clock enable flag
     volatile uint32_t dummy = RCC->APB1ENR1; // read back 
     (void)dummy; // avoid "unused" warning

    hth

    KnarfB

    SSaiy.1
    SSaiy.1Author
    Associate III
    February 13, 2023

    @KnarfB​ yes CNT is updating.

    KnarfB
    Super User
    February 13, 2023

    Any other init code before? Works "as is" on my Nucleo-STM32L432KC (LED on PB3) when started from first line in main()

    hth

    KnarfB

    SSaiy.1
    SSaiy.1Author
    Associate III
    February 13, 2023

    Nothing except the code I updated here.

    SSaiy.1
    SSaiy.1Author
    Associate III
    February 14, 2023

    When I tried with Timer 2 this code is working as expected, LED blinks at 1 second interval. Is the Timer 6 of STM32L412 has any additional configuration to made in order to work like this.

    This is what I get when I debug.

    0693W00000YAfEFQA1.png

    KnarfB
    Super User
    February 14, 2023

    This happens when the specific IRQ handler is not implemented. See the interrupt vector table in the startup code for the proper names. Guess: TIM6_DAC_IRQHandler?

    hth

    KnarfB

    waclawek.jan
    Super User
    February 14, 2023

    > See the interrupt vector table in the startup code for the proper names.

    +1

    I wonder where startup_stm32l412rbtx.s is from - not from https://github.com/STMicroelectronics/STM32CubeL4/tree/master/Drivers/CMSIS/Device/ST/STM32L4xx/Source/Templates

    General "interrupt does not fire" troubleshooting steps here.

    JW

    SSaiy.1
    SSaiy.1Author
    Associate III
    February 14, 2023

    when I tried the debug mode startup_stm32l412rbtx.s was autoloading because of the error, it was in the debug folder under projectname.elf -[arm/le]. I got the Handler name from this file.

    0693W00000YAgnaQAD.png

    KnarfB
    Super User
    February 14, 2023

    What toolchain / version are you using?

    KnarfB

    SSaiy.1
    SSaiy.1AuthorBest answer
    Associate III
    February 14, 2023

    Thanks @KnarfB as you said IRQ handler was different the actual one is TIM6_DACUNDER_IRQHandler. After I changed the handler name the code started working

    KnarfB
    Super User
    February 14, 2023

    Glad it works. To add some confusion: stm32l412xx.h (ARM CMSIS) and others contains a line

    /* Aliases for __IRQHandler */
    #define TIM6_IRQHandler TIM6_DAC_IRQHandler

    which covers that error up. But you don't seem to use that.

    KnarfB