Skip to main content
Associate II
Mar 16, 2026 11:54 AM UTC
Question

Status of USART, SPI and CAN in ST bootloader for STM32L4 ?

New question split from this post.

One additinal request: When checking if bootloader pin configuration has an impact on the real application it would be helpful to know the default level for output pins, like

  • does the UART_TX pin drive active high or low?
  • does the boot loader drive the SPI MISO output pin HI, LO or Z?
  • is the CAN_TX pin drven HI or LOW?

Thank you!

2 replies

mƎALLEm
ST Technical Moderator
Mar 16, 2026 12:10 PM UTC

That's a new question that needs to be separated.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
Sep 2, 2026 9:46 AM UTC

Hello,

Asking that question internally over the ticket number CDM0065494 (not accessible by the community users). I’ll get back to you as soon as I have a feedback.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.