Skip to main content
Associate II
March 25, 2024
Question

Setting up HyperRAM S70KL1282 with STM32H735 issues

  • March 25, 2024
  • 22 replies
  • 7944 views

Hi,

I'm trying to setup this new RAM chips on STM32H735 in OSPI/HyperRAM mode. The HW connection is the same as on ST STM32H735 devkit. I found a driver for similar chip S70KL1281 but there are some differences, e.g. in latencies, but generally S70KL1282 is faster. The used driver file identification from header:

******************************************************************************
* @file s70kl1281.c
* @modify MCD Application Team
* @brief This file provides the S70KL1281 OSPI drivers.

...

* Copyright (c) 2020 STMicroelectronics.
******************************************************************************

I configured the Hyperbus in STM32CubeMX but there are no hints how to setup all the options for this memory. So after some messing and trial-error I ended with this partially working init code:

 

 

static void MX_OCTOSPI2_Init(void)
{
 OSPIM_CfgTypeDef sOspiManagerCfg = {0};
 OSPI_HyperbusCfgTypeDef sHyperBusCfg = {0};

 /* OCTOSPI2 parameter configuration*/
 hospi2.Instance = OCTOSPI2;
 hospi2.Init.FifoThreshold = 1;
 hospi2.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
 hospi2.Init.MemoryType = HAL_OSPI_MEMTYPE_HYPERBUS;
 hospi2.Init.DeviceSize = 24;
 hospi2.Init.ChipSelectHighTime = 1;
 hospi2.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
 hospi2.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
 hospi2.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
 hospi2.Init.ClockPrescaler = 2; // for testing use prescaler 2 at 133MHz, prescaler 1 gets garbage
 hospi2.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
 hospi2.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;
 hospi2.Init.ChipSelectBoundary = 0;
 hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED;
 hospi2.Init.MaxTran = 0;
 hospi2.Init.Refresh = 500;
 if (HAL_OSPI_Init(&hospi2) != HAL_OK)
 {
 Error_Handler();
 }
 sOspiManagerCfg.ClkPort = 2;
 sOspiManagerCfg.DQSPort = 2;
 sOspiManagerCfg.NCSPort = 2;
 sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;
 sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_2_HIGH;
 if (HAL_OSPIM_Config(&hospi2, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }
 sHyperBusCfg.RWRecoveryTime = 3;
 sHyperBusCfg.AccessTime = 7;
 sHyperBusCfg.WriteZeroLatency = HAL_OSPI_NO_LATENCY_ON_WRITE; // someone suggested HAL_OSPI_LATENCY_ON_WRITE but doesn't have effect
 sHyperBusCfg.LatencyMode = HAL_OSPI_FIXED_LATENCY;
 if (HAL_OSPI_HyperbusCfg(&hospi2, &sHyperBusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }
}

 

 

First time I had a problem that reading from memory was unrealiable and I sometimes getting a different results on every run. Enabling the magic option hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED; solved it but still not at the full clock speed I configured - I have both OSPI clocked at 133MHz. The FlashROM at OSPI1 works fine at 133MHz but for this HyperRAM I have to set prescaler 2. Then I got some consistent result.

But there's another problem that test data pattern I wrote into memory are readed by 8 Bytes shifted further than it should be. Currently for testing I don't use mapping yet but I use driver functions S70KL1281_Write and S70KL1281_Read. A simple piece of code for test write and readbeck:

 

 

{
uint8_t buff[64]={0};
int i;
buff[0]=0xab; buff[1]=0xcd; buff[2]=0xef; buff[3]=0xaa;
if (S70KL1281_Write(&XRAM, buff, 0, 16)!=S70KL1281_OK)
 printf("Failed to write to HyperRAM\n");
for (i=0; i<32; i++)
 printf("%02X ", buff[i]);
printf("\n");
if (S70KL1281_Read(&XRAM, buff, 0, 32)!=S70KL1281_OK)
 printf("Failed to read from HyperRAM\n");
for (i=0; i<32; i++)
 printf("%02X ", buff[i]);
printf("\n");
if (S70KL1281_Read(&XRAM, buff, 0, 32)!=S70KL1281_OK)
 printf("Failed to read from HyperRAM\n");
for (i=0; i<32; i++)
 printf("%02X ", buff[i]);
printf("\n");
}

 

 

The memory address is 0 but I get this:

Ext. OctoSPI HyperRAM ID: 0C81 0001
Manufacturer: Infineon, HyperRAM 2.0, rowbits: 13, colbits: 9
AB CD EF AA 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
57 47 57 5D D5 D7 8C 15 AB CD EF AA 00 00 00 00 00 00 00 00 00 00 00 00 D5 D5 57 5F D5 D5 5F 75
57 47 57 5D D5 D7 8C 15 AB CD EF AA 00 00 00 00 00 00 00 00 00 00 00 00 D5 D5 57 5F D5 D5 5F 75

There's some garbage in first 8 Bytes (57 47 57 5D D5 D7 CC 15 - uninitialized memory?) followed by correct pattern AB CD EF AA and trailing zeros from buffer

This topic has been closed for replies.

22 replies

ST Employee
March 25, 2024

Hello @martin,

I checked your OCTOSPI configuration, and it seems correct!

I propose testing this example:STM32CubeH7 OSPI HyperRAM MemoryMapped, and changing the OSPI_HYPERRAM_LATENCY from 6 to 7 in the main.h file (as per the memory datasheet, the default value of the Initial Latency is 7). This example demonstrates how to write to and read data from the OCTOSPI HyperRAM memory in memory-mapped mode and to compare the results with those from intensive access.

The HyperRAM memory used is an S70KL1281.

 

Kind regards,

Nissrine

MartinDQAuthor
Associate II
March 26, 2024

I tried to use S70KL1281_EnableMemoryMappedMode() function from the driver to enable mem.mapping but I'm still having 8B offset. I also tried to use OSPI2 initilaization function parametyers but result was the same. I suspect it must be there some difference between S70KL1281 and S70KL1282...

{
__IO uint32_t *mem_addr = (__IO uint32_t *)(OCTOSPI2_BASE);
int i;

if (S70KL1281_EnableMemoryMappedMode(&XRAM)!=S70KL1281_OK)
 printf("Failed to Enable Memory Mapped Mode\n");
else
 printf("Memory Mapped Mode Enabled\n");

mem_addr[0]=0xABCDEFAA;
mem_addr[1]=0x12345678;
mem_addr[2]=0;
mem_addr[3]=0;
for (i=0; i<48; i++); // a shot delay, 46 read ok, 47 read garbage

printf("%08lX\n", mem_addr[0]);
printf("%08lX\n", mem_addr[0]);
printf("%08lX\n", mem_addr[0]); // 57 45 57 5D = "WEW]"

for (i=0; i<32/4; i++)
 printf("%08lX ", mem_addr[i]);
printf("\n");

for (i=0; i<32; i++)
 printf("%02X ", ((uint8_t *)mem_addr)[i]);
printf("\n");
}

Output is:

Ext. OctoSPI HyperRAM ID: 0C81 0001
Manufacturer: Infineon, HyperRAM 2.0, rowbits: 13, colbits: 9
Memory Mapped Mode Enabled
ABCDEFAA - this read changes according to for loop short delay, for shorter times it reads ABCDEFAA, for longer times it reads 5D574557
5D574557
5D574557
5D574557 158CD7D5 ABCDEFAA 12345678 00000000 00000000 5F57D5D5 755FF5D5
57 45 57 5D D5 D7 8C 15 AA EF CD AB 78 56 34 12 00 00 00 00 00 00 00 00 D5 D5 57 5F D5 F5 5F 75

ST Employee
April 2, 2024

Hello @MartinDQ 

 

I have run a test with an STM32H735G-DK that integrates the HyperRam S70KL1281, using your OSPI2 configuration and the S70KL1281_Write and S70KL1281_Read functions from the S70KL1281 OSPI drivers. With the exception that the access time in my case should be set to 6 for the S70KL1281 memory, I found that the issue is related to the refresh parameter. According to the memory datasheet, this parameter should be 4µs (see section 10.5.2 Write transactions, Table 34 Write timing parameters, page 50).

For this reason, I propose using the following formula to determine the correct value:

 

uint32_t Ospi_clk = HAL_RCCEx_GetPeriphCLKFreq(RCC_PERIPHCLK_OSPI);
OSPIHandle.Init.Refresh = ((2U * (Ospi_clk / (OSPIHandle.Init.ClockPrescaler + 1U))) / 1000000U) + 4U; // The chip select should be released every 4µs

 

 

Kind regards,

Nissrine

LCE
Principal II
March 27, 2024

Hi Martin,

I'm still using the H735-DK with the S70KL1281, planning to use S70KL1282 on my custom PCB.

So for now I can compare your code only to mine with direct register setup, working with S70KL1281 at 100 MHz.

Differences to your code:

- setup: FIFO threshold = 4 (maybe that's worth a try, as some other STM32 Q/O-SPIs suffer from alignment problems)

- delay block, setting the registers:

/* DELAY block */
	/* disable the output clock and enable the access to the phase selection SEL[3:0] */
	DLYB_OCTOSPI1->CR 	= DLYB_CR_SEN;
	/* set delay */
	DLYB_OCTOSPI1->CFGR = (0 & DLYB_CFGR_SEL_Msk);
	/* disable the access to the phase selection, enable output */
	DLYB_OCTOSPI1->CR 	= DLYB_CR_DEN;

- and another good guess: I start "MspInit" with a peripheral reset after the clock enable:

void OctoSpiGpioDmaInit(OSPI_HandleTypeDef *phOspi)
{
	GPIO_InitTypeDef GPIO_InitStruct = { 0 };

	if( OCTOSPI1 == phOspi->Instance )
	{
		/* OCTOSPI1 clock enable */
		__HAL_RCC_OCTOSPIM_CLK_ENABLE();
		__HAL_RCC_OSPI1_CLK_ENABLE();

		/* reset & release */
		__HAL_RCC_OSPI1_FORCE_RESET();
		__HAL_RCC_OSPI1_RELEASE_RESET();

		/** OCTOSPI 1 GPIO Configuration
...

 

 

 

 

MartinDQAuthor
Associate II
March 27, 2024

OK, can you tell me that R/W works as expected for you on S70KL1281? When do you get S70KL1282? I would use S70KL1281 in our project but it was out of stock so I have to choose some newer replacement...

I already tried FIFO threshold = 4 and all options from main.c of example code (begisn with /* Initialize OctoSPI ----------------------------------------------------- */) but any difference. I don't use DMA. I may play with delay block a bit but it seems to be a mystery box. From what I have found it seems that it needs to be tuned differently for various chips, probably by trial error...

LCE
Principal II
March 27, 2024

OK, can you tell me that R/W works as expected for you on S70KL1281?

Yes, using it in memory mapped mode only, it works for hours / days.

Maximum speed depends on compilation (I have to find the reasons for that), it's always above 400 Mbit/s, best write rate was something about 1500 Mbit/s.

I would use S70KL1281 in our project but it was out of stock...

Same here, it's EOL.

Infineon even has a migration datasheet, and the only (seemingly) relevant difference is the latency of 7 instead of 6 cycles.

Alex - APMemory
Associate II
May 15, 2024

fyi, if any issue to source 128Mb OPI 3V BGA24 due to EOL, you can get APS12808L-3OBM-BA (also tested on STM32H72x/3x Disco, file attached)

Alex

Datasheet : http://www.apmemory.com/wp-content/uploads/APS12808L-3OBM-BA.pdf

Proto: https://www.mouser.com/ProductDetail/AP-Memory/APS12808L-3OBM-BA?qs=IS%252B4QmGtzzrXcGkbuYahqw%3D%3D

 

LCE
Principal II
March 27, 2024

When do you get S70KL1282?

I just ordered the PCB incl. assembly, that will take at least 8 weeks from now on. :(

 

MartinDQAuthor
Associate II
March 27, 2024

BTW what clock speed do you use for OSPI and what divider?

I routed it to some PLL output that I set at 133MHz. Before enabling the delay block I got some data consistency issues did you tried also without delay block and how it performed?

I don't have fast-enugh scope to check waveforms at full speed.

I went through the datesheet and already seen the initial latency difference so I set it in my code. Also there's a mention that this memory is duble-die (stacked) chip but I don't know if it imply some different behavior, I think it's just internal architecture that should be transparent for the user who see just a single 32-bit address from the outside...

LCE
Principal II
March 28, 2024

Clock source is RCC_OSPICLKSOURCE_D1HCLK, which is 1/2 system clock, in my case clock sourcing OSPI is 200 MHz, prescaler halves that, so it's running with 100 MHz. Same scope problems here... :D

I played with the delay block in the beginning, then found that best setting was to activate it, but keep all values at 0. It seemed that the propagation delay alone by activation was good enough.

Edit: find my HyperRam setup in attached files, including test function with quite exact time measurement with DWT->CYCCNT
Works on H735-DK with the S70KL1281 at 100 MHz.

In case you never used DWT->CYCCNT, here's the setup:

/* +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
/* CPU cycle count activation for debugging */
#if( 1 ) 	//	DEBUG_CPU_TIMING
	CoreDebug->DEMCR |= CoreDebug_DEMCR_TRCENA_Msk;
	DWT->LAR = 0xC5ACCE55;
	DWT->CYCCNT = 0;
	DWT->CTRL |= DWT_CTRL_CYCCNTENA_Msk;
	DWT->CTRL |= DWT_CTRL_PCSAMPLENA_Msk;
#endif	/* DEBUG_CPU_TIMING */
MartinDQAuthor
Associate II
April 15, 2024

Any chance that some engineer from ST could try the new memory S70KL1282 on the discovery kit?

I think that they will be forced to upgrade anyway as the current part is EoL and will be no longer available. Except they bought a huge amount of old chips so they still have enough spare...

ST Employee
April 16, 2024

Hello @MartinDQ 

 
Currently, the S70KL1282 is not available at my end. However, I will inquire further internally and provide you with an update as soon as possible.
 
Kind regards,
Nissrine. 
LCE
Principal II
April 15, 2024

So it's still not working? :(

I just got the message that will get my prototypes with the S70KL1282 in mid / end june. :(

MartinDQAuthor
Associate II
April 15, 2024

No, refresh settings didn't have any effect on this issue. Currently I'm working on other project so I'll return to this later. I also asked on Infineon forum where they only suggested a change of latency 6->7 that I already did...

Associate III
May 14, 2024

Hello @NesrynELMK 

 

do you have any updates on that issue? We are planning to use the S70KL1282 with the STM32H735 for our product, and are concerned that we could not make the HyperRAM work properly, which would be critical for our design.

 

Thanks and kind regards,

RK_IOT 

ST Employee
May 15, 2024

Hello @rk_iot , @MartinDQ 

I have not received the sample yet, but I will keep you updated once I test it.

In the meantime, @MartinDQ, have you checked that all the signals have the same length ?

You can check the following thread:  Solved: Write/Read issues with HyperRAM S70KL1282 on OctoS... - STMicroelectronics Community. It may help you.

 

Kind regards