Skip to main content
Associate II
March 25, 2024
Question

Setting up HyperRAM S70KL1282 with STM32H735 issues

Hi,

I'm trying to setup this new RAM chips on STM32H735 in OSPI/HyperRAM mode. The HW connection is the same as on ST STM32H735 devkit. I found a driver for similar chip S70KL1281 but there are some differences, e.g. in latencies, but generally S70KL1282 is faster. The used driver file identification from header:

******************************************************************************
* @file s70kl1281.c
* @modify MCD Application Team
* @brief This file provides the S70KL1281 OSPI drivers.

...

* Copyright (c) 2020 STMicroelectronics.
******************************************************************************

I configured the Hyperbus in STM32CubeMX but there are no hints how to setup all the options for this memory. So after some messing and trial-error I ended with this partially working init code:

 

 

static void MX_OCTOSPI2_Init(void)
{
 OSPIM_CfgTypeDef sOspiManagerCfg = {0};
 OSPI_HyperbusCfgTypeDef sHyperBusCfg = {0};

 /* OCTOSPI2 parameter configuration*/
 hospi2.Instance = OCTOSPI2;
 hospi2.Init.FifoThreshold = 1;
 hospi2.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
 hospi2.Init.MemoryType = HAL_OSPI_MEMTYPE_HYPERBUS;
 hospi2.Init.DeviceSize = 24;
 hospi2.Init.ChipSelectHighTime = 1;
 hospi2.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
 hospi2.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
 hospi2.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
 hospi2.Init.ClockPrescaler = 2; // for testing use prescaler 2 at 133MHz, prescaler 1 gets garbage
 hospi2.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
 hospi2.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;
 hospi2.Init.ChipSelectBoundary = 0;
 hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED;
 hospi2.Init.MaxTran = 0;
 hospi2.Init.Refresh = 500;
 if (HAL_OSPI_Init(&hospi2) != HAL_OK)
 {
 Error_Handler();
 }
 sOspiManagerCfg.ClkPort = 2;
 sOspiManagerCfg.DQSPort = 2;
 sOspiManagerCfg.NCSPort = 2;
 sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;
 sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_2_HIGH;
 if (HAL_OSPIM_Config(&hospi2, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }
 sHyperBusCfg.RWRecoveryTime = 3;
 sHyperBusCfg.AccessTime = 7;
 sHyperBusCfg.WriteZeroLatency = HAL_OSPI_NO_LATENCY_ON_WRITE; // someone suggested HAL_OSPI_LATENCY_ON_WRITE but doesn't have effect
 sHyperBusCfg.LatencyMode = HAL_OSPI_FIXED_LATENCY;
 if (HAL_OSPI_HyperbusCfg(&hospi2, &sHyperBusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }
}

 

 

First time I had a problem that reading from memory was unrealiable and I sometimes getting a different results on every run. Enabling the magic option hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED; solved it but still not at the full clock speed I configured - I have both OSPI clocked at 133MHz. The FlashROM at OSPI1 works fine at 133MHz but for this HyperRAM I have to set prescaler 2. Then I got some consistent result.

But there's another problem that test data pattern I wrote into memory are readed by 8 Bytes shifted further than it should be. Currently for testing I don't use mapping yet but I use driver functions S70KL1281_Write and S70KL1281_Read. A simple piece of code for test write and readbeck:

 

 

{
uint8_t buff[64]={0};
int i;
buff[0]=0xab; buff[1]=0xcd; buff[2]=0xef; buff[3]=0xaa;
if (S70KL1281_Write(&XRAM, buff, 0, 16)!=S70KL1281_OK)
 printf("Failed to write to HyperRAM\n");
for (i=0; i<32; i++)
 printf("%02X ", buff[i]);
printf("\n");
if (S70KL1281_Read(&XRAM, buff, 0, 32)!=S70KL1281_OK)
 printf("Failed to read from HyperRAM\n");
for (i=0; i<32; i++)
 printf("%02X ", buff[i]);
printf("\n");
if (S70KL1281_Read(&XRAM, buff, 0, 32)!=S70KL1281_OK)
 printf("Failed to read from HyperRAM\n");
for (i=0; i<32; i++)
 printf("%02X ", buff[i]);
printf("\n");
}

 

 

The memory address is 0 but I get this:

Ext. OctoSPI HyperRAM ID: 0C81 0001
Manufacturer: Infineon, HyperRAM 2.0, rowbits: 13, colbits: 9
AB CD EF AA 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
57 47 57 5D D5 D7 8C 15 AB CD EF AA 00 00 00 00 00 00 00 00 00 00 00 00 D5 D5 57 5F D5 D5 5F 75
57 47 57 5D D5 D7 8C 15 AB CD EF AA 00 00 00 00 00 00 00 00 00 00 00 00 D5 D5 57 5F D5 D5 5F 75

There's some garbage in first 8 Bytes (57 47 57 5D D5 D7 CC 15 - uninitialized memory?) followed by correct pattern AB CD EF AA and trailing zeros from buffer

This topic has been closed for replies.

22 replies

LCE
Principal III
May 14, 2024

@MartinDQ & @NesrynELMK 

I'm also curious...

@rk_iot 
I'll get some custom boards with H733 + S70KL1282 in June, then I will be able to test.

The good thing: there are a few pin-compatible octal SPI / HyperRam devices available from other companies.
But I hope it will be possible to make it work... ;) 

MartinDQAuthor
Associate II
May 14, 2024

Hi, sorry, I'm currently working on another PCB design project so I didn't debug it further. But I got some sample code from Infineon for this memory chip and a bit different STM32 MCU that is claimed to work. I hope I'll have a time to try it out soon, I'll post the result here too.

MartinDQAuthor
Associate II
May 15, 2024

Yes I did take a care about QSPI length matching but on such relative low frequencies it doesn't matter much... Even I tried lowering QSPI clock frequency and it has no effect.

LCE
Principal III
June 7, 2024

I got my custom PCB today, including H733 and S70KL1282.

At least the HyperRam worked instantly. 

I check at power up by completely writing the RAM with i = 0, i++, then reading it back. 
I know this test is not perfect, but on my test boards until now, when this test was working, so did the audio / SAI buffers I used in HyperRAM.

I think the only change compared to S70KL1281 was setting the latency to 7.

See init below.

 

/* +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
/* OCTOSPIx basic init function
 *	for octal HyperBus / HyperRAM
 *	Infineon S70KL1281 / S70KL1282
 *		in memory-mapped mode
 *		linear burst read & write => no page wrap (only at end of memory)
 * 	input clock is 1/2 HCLK (200 MHz) -> prescaler /2
 */
uint8_t OspiHypRam_Init(void)
{
	uint8_t u8RetVal = 0;

	/* use pointer to simplify OSPI 1 / 2 switching */
#if OSPI_CUSTOM_RAM_OSPI1 // custom: OSPI 1 HyperRAM; OSPI 2 Quad Flash
	pOspiHypRam = OCTOSPI1;
#else							// H735D: OSPI 1 Oct Flash; OSPI 2 HyperRAM
	pOspiHypRam = OCTOSPI2;
#endif	/* OSPI_CUSTOM_RAM_OSPI1 */

	hOspiHypRam.Instance = pOspiHypRam;

	/* clock & GPIO initialization */
	OspiHypRamGpioDmaInit();

	/* start OFF */
	pOspiHypRam->CR = 0;

/* DEVICE configuration registers
 *	DCR1 .. DCR4
 */

	/* DCR1:
	 *	MTYP 	= 100	Hyperbus memory mode
	 *	DEVSIZE
	 *	CHST
	 *	DLYBYP 	= 0		delay block is used
	 *	FRCK 	= 0		no free running clock
	 *	CKMODE 	= 0		clock low when idle
	 */
	pOspiHypRam->DCR1 =	OCTOSPI_DCR1_MTYP_2 |
						((OSPI_HYPERRAM_SIZE - 1) << OCTOSPI_DCR1_DEVSIZE_Pos) |
						((OSPI_HYPERRAM_NCS_HITIME - 1) << OCTOSPI_DCR1_CSHT_Pos);

	/* DCR2:
	 *	WRAPSIZE 	= 0 	wrapped read OFF
	 *	PRESCALER 	= 1 	divide by 2 -> 100 MHz = max at 3.3V
	 */
	pOspiHypRam->DCR2 = (OSPI_HYPERRAM_WRAP_ZERO << OCTOSPI_DCR2_WRAPSIZE_Pos) |
						((OSPI_HYPERRAM_CLK_DIV - 1) << OCTOSPI_DCR2_PRESCALER_Pos);

	/* DCR3:
	 *	CSBOUND 	= 23 	set to 2^n memory size
	 *	MAXTRAN 	= 0 	unused
	 */
	pOspiHypRam->DCR3 = (OSPI_HYPERRAM_CSBOUND << OCTOSPI_DCR3_CSBOUND_Pos);

	/* DCR4:
	 *	REFRESH 	= 400 	NCS must be released for PSRAM for internal refresh
	 */
	pOspiHypRam->DCR4 = OSPI_HYPERRAM_REFRESH;


/* CR: control register
 *	no polling
 *	no interrupts
 *	FMODE 	= 0		indirect mode, set to memory-mapped mode later
 *	FTTHRES	= 4		FIFO threshold
 *	FSEL 	= 0		nc in octal mode
 *	TCEN 	= 0		no timeout counter
 *	DMAEN 	= 0		no DMA
 *	ABORT 	= 0		no ABORT request
 *	EN 		= 0		ENable set later
 */
	pOspiHypRam->CR =	((OSPI_HYPERRAM_FTHRES - 1) << OCTOSPI_CR_FTHRES_Pos);

/* TCR: timing config
 *	SSHIFT 	= 0 	no read sample shifting
 *	DHQC 	= 1 	delay hold quarter cycle ON
 *	DCYC 	= 0 	dummy cycles between readd addr & data
 */
	pOspiHypRam->TCR = 	OCTOSPI_TCR_DHQC |
						(OSPI_HYPERRAM_DCYC << OCTOSPI_TCR_DCYC_Pos);

/* Hyperbus configuration
 *	memory-mapped mode configuration
 *	CR, DCR1, CCR, WCCR, DLR, AR
 */

	/* HLCR: HyperBus latency configuration register
	 *	TRWR[7:0]	= x		read write recovery time
	 *	TACC[7:0]	= y		access time
	 *	WZL			= 0		latency on write access
	 *	LM			= 1		fixed latency
	 */
	pOspiHypRam->HLCR = (OSPI_HYPERRAM_RW_REC_TIME << OCTOSPI_HLCR_TRWR_Pos) |
						(OSPI_HYPERRAM_LATENCY << OCTOSPI_HLCR_TACC_Pos) |
						OCTOSPI_HLCR_LM;

	/* CR: clear FMODE -> exit MM for now */
	pOspiHypRam->CR 	&= ~OCTOSPI_CR_FMODE;

	/* DCR1: Hyperbus from register access to memory */
	pOspiHypRam->DCR1 	&= ~OCTOSPI_DCR1_MTYP_0;

	/* CCR & WCCR:
	 *	DQS signal enabled (used as RWDS)
	 *	DTR mode enabled on address and data
	 *	address and data on 8 lines
	 */
	/* READ: CCR */
	pOspiHypRam->CCR = 	OCTOSPI_CCR_DQSE |
						OCTOSPI_CCR_DDTR | OCTOSPI_CCR_DMODE_2 |
						OCTOSPI_CCR_ADSIZE | OCTOSPI_CCR_ADDTR | OCTOSPI_CCR_ADMODE_2;

	/* WRITE: WCCR */
	pOspiHypRam->WCCR = OCTOSPI_CCR_DQSE |
						OCTOSPI_WCCR_DDTR | OCTOSPI_WCCR_DMODE_2 |
						OCTOSPI_WCCR_ADSIZE | OCTOSPI_WCCR_ADDTR | OCTOSPI_WCCR_ADMODE_2;

	/* DLR: data length = 1 byte */
	pOspiHypRam->DLR	= 0;

	/* AR: address reset */
	pOspiHypRam->AR		= 0;

	/* update state */
	hOspiHypRam.State 	= HAL_OSPI_STATE_CMD_CFG;

	/* LPTR: lo-power timeout reset */
	pOspiHypRam->LPTR 	= 0;

/* ++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
/* HW IO MUX setup */

	/* MUX OCTOSPIM->PCR[n] */
	pOspiHypRam->CR 	&= ~OCTOSPI_CR_EN;

	/* NO multiplexed mode */
	OCTOSPIM->CR		= 0;

#if OSPI_CUSTOM_RAM_OSPI1 		// custom: OSPI 1 HyperRAM; OSPI 2 Quad Flash

	/* PORT 1:
	 *	select signals & enable
	 *	hi port 1 4..7: OCTOSPIM_PCR_IOHsrc=01 + IOHEN
	 *	lo port 1 0..3: OCTOSPIM_PCR_IOLsrc=00 + IOLEN
	 *	NCS 1: NCSsrc=0 + NCSEN
	 *	DQS 1: DQSsrc=0 + DQSEN
	 *	CLK 1: CLKsrc=0 + CLKEN
	 */
	OCTOSPIM->PCR[0] = ( 	OCTOSPIM_PCR_IOHSRC_0 | OCTOSPIM_PCR_IOHEN |
							OCTOSPIM_PCR_IOLEN |
							OCTOSPIM_PCR_NCSEN |
							OCTOSPIM_PCR_DQSEN |
							OCTOSPIM_PCR_CLKEN );

/* DELAY block */
	/* disable the output clock and enable the access to the phase selection SEL[3:0] */
	DLYB_OCTOSPI1->CR 	= DLYB_CR_SEN;
	/* set delay */
	DLYB_OCTOSPI1->CFGR = (0 & DLYB_CFGR_SEL_Msk);
	/* disable the access to the phase selection, enable output */
	DLYB_OCTOSPI1->CR 	= DLYB_CR_DEN;

#else							// H735-DK: OSPI 1 Oct Flash; OSPI 2 HyperRAM

	/* PORT 2:
	 *	select signals & enable
	 *	hi port 2 4..7
	 *	lo port 2 0..3
	 *	NCS 2
	 *	DQS 2
	 *	clock 2
	 */
	OCTOSPIM->PCR[1] = ( 	OCTOSPIM_PCR_IOHSRC_1 | OCTOSPIM_PCR_IOHSRC_0 | OCTOSPIM_PCR_IOHEN |
							OCTOSPIM_PCR_IOLSRC_1 | OCTOSPIM_PCR_IOLEN |
							OCTOSPIM_PCR_NCSSRC | OCTOSPIM_PCR_NCSEN |
							OCTOSPIM_PCR_DQSSRC | OCTOSPIM_PCR_DQSEN |
							OCTOSPIM_PCR_CLKSRC | OCTOSPIM_PCR_CLKEN );

/* DELAY block */
	/* disable the output clock and enable the access to the phase selection SEL[3:0] */
	DLYB_OCTOSPI2->CR 	= DLYB_CR_SEN;
	/* set delay */
	DLYB_OCTOSPI2->CFGR = (0 & DLYB_CFGR_SEL_Msk);
	/* disable the access to the phase selection, enable output */
	DLYB_OCTOSPI2->CR 	= DLYB_CR_DEN;

#endif	/* OSPI_CUSTOM_RAM_OSPI1 */

	/* enable in peripheral -> clear bypass */
	pOspiHypRam->DCR1 &= ~OCTOSPI_DCR1_DLYBYP;

/* clear all status flags */
	pOspiHypRam->FCR = 0xFFFFFFFF;

/* CR: memory-mapped, no timeout */
	pOspiHypRam->CR 	&= ~OCTOSPI_CR_TCEN;
	pOspiHypRam->CR 	|= OCTOSPI_CR_FMODE;
/* CR: enable peripheral */
	pOspiHypRam->CR 	|= OCTOSPI_CR_EN;

	/* set state (for DMA & HAL stuff) */
	hOspiHypRam.State = HAL_OSPI_STATE_BUSY_MEM_MAPPED;

	return u8RetVal;
}


/* +++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
/* basic GPIO & DMA init */
void OspiHypRamGpioDmaInit(void)
{
	GPIO_InitTypeDef GPIO_InitStruct = { 0 };

#if OSPI_CUSTOM_RAM_OSPI1 		// custom: OSPI 1 HyperRAM; OSPI 2 Quad Flash

	/* OCTOSPI1 clock enable */
	if( 0 == (RCC->AHB3ENR & RCC_AHB3ENR_IOMNGREN) ) __HAL_RCC_OCTOSPIM_CLK_ENABLE();
	if( 0 == (RCC->AHB3ENR & RCC_AHB3ENR_OSPI1EN) ) __HAL_RCC_OSPI1_CLK_ENABLE();

	/* reset & release */
	__HAL_RCC_OSPI1_FORCE_RESET();
	__HAL_RCC_OSPI1_RELEASE_RESET();

#else	// H735-DK: OSPI 1 Oct Flash; OSPI 2 HyperRAM

	/* OCTOSPI2 clock enable */
	if( 0 == (RCC->AHB3ENR & RCC_AHB3ENR_IOMNGREN) ) __HAL_RCC_OCTOSPIM_CLK_ENABLE();
	if( 0 == (RCC->AHB3ENR & RCC_AHB3ENR_OSPI2EN) ) __HAL_RCC_OSPI2_CLK_ENABLE();

	/* reset */
	__HAL_RCC_OSPI2_FORCE_RESET();
	__HAL_RCC_OSPI2_RELEASE_RESET();

#endif	/* OSPI_CUSTOM_RAM_OSPI1 */

/*
	ATTENTION: very different ALTERNATE function numbers!

	custom: HyperRAM OCTOSPI 1 GPIO Configuration
	PA3		------> OCTOSPIM_P1_CLK
	PB2		------> OCTOSPIM_P1_DQS
	PE11	------> OCTOSPIM_P1_NCS
	PB1		------> OCTOSPIM_P1_IO0
	PB0		------> OCTOSPIM_P1_IO1
	PB13	------> OCTOSPIM_P1_IO2
	PA6		------> OCTOSPIM_P1_IO3
	PE7		------> OCTOSPIM_P1_IO4
	PE8		------> OCTOSPIM_P1_IO5
	PE9		------> OCTOSPIM_P1_IO6
	PE10	------> OCTOSPIM_P1_IO7

	H735-DK: HyperRAM OCTOSPI 2 GPIO Configuration
	PF4 	------> OCTOSPIM_P2_CLK
	PF12	------> OCTOSPIM_P2_DQS
	PG12	------> OCTOSPIM_P2_NCS
	PF0 	------> OCTOSPIM_P2_IO0
	PF1 	------> OCTOSPIM_P2_IO1
	PF2 	------> OCTOSPIM_P2_IO2
	PF3 	------> OCTOSPIM_P2_IO3
	PG0 	------> OCTOSPIM_P2_IO4
	PG1 	------> OCTOSPIM_P2_IO5
	PG10	------> OCTOSPIM_P2_IO6
	PG11	------> OCTOSPIM_P2_IO7
*/

	GPIO_InitStruct.Mode 		= GPIO_MODE_AF_PP;
	GPIO_InitStruct.Pull 		= GPIO_NOPULL;
	GPIO_InitStruct.Speed 		= GPIO_SPEED_FREQ_VERY_HIGH;

/* control signals */

	GPIO_InitStruct.Pin 		= OSPIRAM_CLK_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_CLK_AF;
	HAL_GPIO_Init(OSPIRAM_CLK_GPIO_Port, &GPIO_InitStruct);

	GPIO_InitStruct.Pin 		= OSPIRAM_DQS_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_DQS_AF;
	HAL_GPIO_Init(OSPIRAM_DQS_GPIO_Port, &GPIO_InitStruct);

	GPIO_InitStruct.Pin 		= OSPIRAM_NCS_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_NCS_AF;
	HAL_GPIO_Init(OSPIRAM_NCS_GPIO_Port, &GPIO_InitStruct);

/* data IOs */

	GPIO_InitStruct.Pin 		= OSPIRAM_IO0_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_IO0_AF;
	HAL_GPIO_Init(OSPIRAM_IO0_GPIO_Port, &GPIO_InitStruct);

	GPIO_InitStruct.Pin 		= OSPIRAM_IO1_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_IO1_AF;
	HAL_GPIO_Init(OSPIRAM_IO1_GPIO_Port, &GPIO_InitStruct);

	GPIO_InitStruct.Pin 		= OSPIRAM_IO2_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_IO2_AF;
	HAL_GPIO_Init(OSPIRAM_IO2_GPIO_Port, &GPIO_InitStruct);

	GPIO_InitStruct.Pin 		= OSPIRAM_IO3_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_IO3_AF;
	HAL_GPIO_Init(OSPIRAM_IO3_GPIO_Port, &GPIO_InitStruct);

	GPIO_InitStruct.Pin 		= OSPIRAM_IO4_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_IO4_AF;
	HAL_GPIO_Init(OSPIRAM_IO4_GPIO_Port, &GPIO_InitStruct);

	GPIO_InitStruct.Pin 		= OSPIRAM_IO5_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_IO5_AF;
	HAL_GPIO_Init(OSPIRAM_IO5_GPIO_Port, &GPIO_InitStruct);

	GPIO_InitStruct.Pin 		= OSPIRAM_IO6_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_IO6_AF;
	HAL_GPIO_Init(OSPIRAM_IO6_GPIO_Port, &GPIO_InitStruct);

	GPIO_InitStruct.Pin 		= OSPIRAM_IO7_Pin;
	GPIO_InitStruct.Alternate 	= OSPIRAM_IO7_AF;
	HAL_GPIO_Init(OSPIRAM_IO7_GPIO_Port, &GPIO_InitStruct);
}

/* ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
/* HyperRAM memory:
 *	S70KL1281 on H735-Discovery
 *	S70KL1282 on custom board
 */

/* size 2^x */
#define OSPI_HYPERRAM_SIZE 		24

/* NCS high time between commands */
#define OSPI_HYPERRAM_NCS_HITIME		8

#define OSPI_HYPERRAM_WRAP_ZERO			0

/* clock prescaler */
#define OSPI_HYPERRAM_CLK_DIV			2

#define OSPI_HYPERRAM_CSBOUND			(OSPI_HYPERRAM_SIZE - 1)

#define OSPI_HYPERRAM_REFRESH			400
#define OSPI_HYPERRAM_FTHRES			4
#define	OSPI_HYPERRAM_DCYC				0

/* timing for register HLCR HyperBus latency configuration */
/* clock cycles for read / write recovery time */
#define OSPI_HYPERRAM_RW_REC_TIME		3

/* clock cycles for device access time */
#define OSPI_HYPERRAM_LATENCY_S70KL1281		6
#define OSPI_HYPERRAM_LATENCY_S70KL1282		7

#define OSPI_HYPERRAM_LATENCY		OSPI_HYPERRAM_LATENCY_S70KL1282

/* end address */
#define OSPI_HYPERRAM_END_ADDR 	(1 << OSPI_HYPERRAM_SIZE)


/* ++++++++++++++++++++++++++++++++++++++++++++++++ */
/* DCR2 clock prescaler */

/* functional modes of peripheral */
#define OSPI_CR_FM_INDIRECT_WRITE	(uint32_t)0						/*!< Indirect write mode */
#define OSPI_CR_FM_INDIRECT_READ 	(uint32_t)OCTOSPI_CR_FMODE_0	/*!< Indirect read mode */
#define OSPI_CR_FM_AUTO_POLLING 	(uint32_t)OCTOSPI_CR_FMODE_1	/*!< Automatic polling mode */
#define OSPI_CR_FM_MEMORY_MAPPED 	(uint32_t)OCTOSPI_CR_FMODE		/*!< Memory-mapped mode */

 

Alex - APMemory
Associate II
June 7, 2024

Hi, 

Good to hear, I can't comment much about specific for HyperRAM. 

If competiveness is important, I can just advice to look at APMemory products, APS12808L-3OBM-BA, this is compatible device on your BGA24  PCB footprint.

Regards

Alex