Skip to main content
This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 11, 2024 6:36 PM UTC

Hello @Mimikakarlo and welcome to the community,

According to the datasheet yes and you need to drive it with LTDC interface over RGB lines.

For more details please refer to the AN4861 "Introduction to LCD TFT display controller LTDC on STM32 MCUs"

Hope it helps.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

8 replies

Andrew Neil
Super User
Dec 11, 2024 12:23 PM UTC

@Mimikakarlo wrote:

 RK043FN8H-CT672B 


Are you talking about this display?

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/display-rk043fn66hs-ctg-from-rocktech/td-p/303812

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
Dec 11, 2024 5:56 PM UTC

yes

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 11, 2024 6:36 PM UTC

Hello @Mimikakarlo and welcome to the community,

According to the datasheet yes and you need to drive it with LTDC interface over RGB lines.

For more details please refer to the AN4861 "Introduction to LCD TFT display controller LTDC on STM32 MCUs"

Hope it helps.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate
Dec 11, 2024 6:46 PM UTC

Thank you for youe answer. I have a problem with the RK043FN66HS-CTG display because i want brightness 1000cm/m^2, can you suggest me another display for STM32F756BGT6 with 4.3in, 480 x 272 pixels and 1000cm/m^2?
Thank you!

mƎALLEm
ST Technical Moderator
Dec 11, 2024 10:42 PM UTC

This is what is used on STM32H743-Eval board: AM-640480G5TNQW-T00H

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.