Skip to main content
Associate II
Feb 4, 2024 4:14 PM UTC
Question

printf() on NUCLEO-F767ZI board not working

I had written a function to support printf() using USART3 for NUCLEO-F767ZI board. Please check the code below, but I did not see the prints on the console in STM32CudeIDE. Please let me know what the issue can be. Do I need to do any changes on the board to make it work?

 

int _write(int file, char *ptr, int len)

{

HAL_UART_Transmit(&huart3, (uint8_t*)ptr, len, HAL_MAX_DELAY);

return len;

}

This topic has been closed for replies.

2 replies

STTwo-32
ST Technical Moderator
Feb 4, 2024 5:46 PM UTC

Hello @rdevisetti 

I suggest you to take a look at the FAQ: "How to redirect the printf function to a UART for debug messages"

Best regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Feb 5, 2024 9:49 AM UTC

Before trying to integrate that into printf(), do you have the UART working on its own?

If the UART doesn't work on its own, it's not going to work via printf !

 

Use this button to properly post source code:

AndrewNeil_0-1707132689130.png

 

To get that extra row of icons, press this button:

AndrewNeil_1-1707132689130.png

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.