Skip to main content
Lmyle.11
Associate II
Aug 5, 2020 2:43 PM UTC
Question

On the STM32 can you have JTAG and ETM active at the same time ?or would you need to switch? or does only one need to be activated at any one time? Thanks

..

This topic has been closed for replies.

2 replies

dave2012
Associate III
Aug 5, 2020 5:26 PM UTC

Lmyle,

JTAG and ETM are used concurrently, it's not one or the other. Unless you configure ETM in your firmware application (very unlikely) then it needs to be set-up using JTAG/SWD.

As @clive1 (NFA Crew) says, you'll be able to emulate most if not all of the STM32F413 features with several of the STM32F4xx eval. boards. To use ETM, it needs the 20 way 0.05" pitch trace/JTAG header. Our low cost QTrace probe supports ETM tracing for the F2/F3/F4/L4/F7 parts.

Regards

Dave Bryan

https://www.pdqlogic.com

Tesla DeLorean
Guru
Aug 5, 2020 5:46 PM UTC

This is the original thread, perhaps best to keep things together

https://community.st.com/s/question/0D53W00000EH2IdSAL

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..