Skip to main content
Associate III
November 13, 2025
Question

OCTA SPI PINs For STM32U575VIT6Q Controllers

Hi @Issamos 

Hope You doing well .

 we are started new design using STM32U575VIT6Q this controller, we have some doubts regarding the SPI line, we searched in the STM32cubemx in that we cannot able to find the octa spi pins, Can you pls share me the Standard SPI lines pins and Octa SPI pins ,

thanks 

2 replies

HA2375-Author
Associate III
November 13, 2025

@Issamos

thanks.

ST Technical Moderator
November 13, 2025

Hello @HA2375- 

Please refer to the product's STM32U575 datasheet in table 27 to be able to identify the pins assignment (for exact free/usable pins)

  • SPI2_NSS: PD0, PI0..
  • SPI2_SCK: PD1, PD3, PI1..
  • SPI2_MISO: PD3, PI2..
  • SPI2_MOSI: PD4..
  • SPI3_NSS: PG12
  • SPI3_SCK: PG9
  • SPI3_MISO: PG10
  • SPI3_MOSI: PG11
  • ...

 

ImenD_0-1763038689029.png

There are multiple SPI and OctoSPI pin options, with assignments and you can use STM32CubeMX to configure and remap the alternate functions as needed:

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks