Skip to main content
Associate II
July 3, 2024
Solved

Nucleo-F767ZI does not have able to shockproof or anti-vibration?

Hello everyone,

I used Nucleo-F767ZI board for my vehicle robot. I just securely attach the board to the robot and then testing my robot move on different terrains.

After this test, I can not connect ST-Link (fail.txt file appeared) and my board did not operate anymore. 

I tried to press RESET button or upgrade ST-Link firmware, reconnect USB cable or even reset my computer but nothing worked.

I believe this board dead. 

My question: Does ST have documents on shock protection or anti-vibration standards for the Nucleo board?

Do I need to install an additional damping system for the board?

 

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
July 3, 2024

@ManhPham The STM32 itself are designed for industrial applications, but not the evaluation tools. If you need something rugged, you would have to develop your own suitable board.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

7 replies

Peter BENSCH
ST Technical Moderator
July 3, 2024

NUCLEO boards are evaluation tools that are released for rapid prototyping but not for end applications (see Terms of Use). However, since all documents (layout, schematics, etc.) of the NUCLEO boards are openly accessible, you are free to find a possible cause for the failure.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ManhPhamAuthor
Associate II
July 3, 2024

can you share what ST products are designed for industrial application?

Andrew Neil
Super User
July 3, 2024

Maybe this: https://www.st.com/en/evaluation-tools/steval-stwinkt1b.html ?

But remember that, in general,  ST's products are components - for customers to design-in to their own products.

Things like Nucleo, Discovery, and DK boards are just tools to aid in evaluation & development.

If you're looking for ready-to-deploy products, you should be looking to 3rd-parties.

There are many 3rd-party robot controllers...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
July 3, 2024

@ManhPham wrote:

I can not connect ST-Link (fail.txt file appeared) 


Give more details of the nature of this failure.

What is this "fail.txt"? Where did it "appear"? What did it contain?

Does the ST-Link show up in the PC's Device Manager (or equivalent)?

Take a look at this Knowledgebase article:

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/ta-p/49693

 


@ManhPham wrote:

Does ST have documents on shock protection or anti-vibration standards for the Nucleo board?


As @Peter BENSCH said, the Nucleo boards are for evaluation use - on a desk / in a lab - they are not "rugged"

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
July 3, 2024

@ManhPham The STM32 itself are designed for industrial applications, but not the evaluation tools. If you need something rugged, you would have to develop your own suitable board.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
July 3, 2024

The NUCLEO, EVAL and DISCO boards have about zero consideration for industrial usage

The power and USB connectors aren't particularly robust, it's likely you shorted something out, or had excessive voltage from external connections.

 

Perhaps look at UAV FLIGHT CONTROLLER boards, and soldered / stress-relieved cable connectivity.

Look for third party boards targeting industrial and automotive applications, they are likely to be significantly more expensive.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
July 3, 2024

@Tesla DeLorean wrote:

The ... USB connectors aren't particularly robust.


Indeed - have had these fail even just on "desktop" use.

@ManhPham Did you have the USB plugged-in while your robot was running on the rough terrain? If so, quite likely that it's failed

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.