Skip to main content
Uwe Bonnes
Chief
Nov 6, 2025 3:37 PM UTC
Question

Missing STM32U5 kernel clock limits

For H7, the kernel clock limit are given in Table 61 Kernel clock distribution overview as shown in

https://community.st.com/t5/stm32cubemx-mcus/stm32h745-fdcan-clock-frequency/td-p/83540

I do not find a similar table for U5 in the most recent datasheets and reference manual. If I did not look carefully enough, any hint to find it is welcome. Otherwise ST should  consider adding like for H7.

5 replies

MKANO.2
ST Employee
Nov 10, 2025 11:22 AM UTC

Hello @Uwe Bonnes 

For the STM32U5, all details regarding the kernel clocks are provided in the RCC chapter and illustrated in the Clock Tree figure.

Best regards

Mariem

Uwe Bonnes
Chief
Nov 10, 2025 12:49 PM UTC

So please tell me where exactly to find in rm0456 RCC chapter the limits for the FDCAN kernel clock!

MKANO.2
ST Employee
Nov 10, 2025 2:17 PM UTC

When selecting pll1_q_ck as the kernel clock for FDCAN, the maximum frequency is 160 MHz , as detailed in the Datasheet’s PLL Characteristics table. This specification is also reflected in CubeMX.

Uwe Bonnes
Chief
Nov 10, 2025 2:53 PM UTC

We have a differing understanding of the meaning of reference manual. For me, a "reference manual" should be the reference and not some tools where with some input and click you can get some information that you can believe or not but you can not check the values against the reference manual.

mƎALLEm
ST Technical Moderator
Nov 11, 2025 2:29 PM UTC

Hello @Uwe Bonnes 

I'm asking that question internally for STM32U5. I'm getting back to you as soon I have an answer. Internal ticket number 221521.

In fact the same table is provided for STM32H5 product in the datasheet:

mALLEm_0-1762871352245.png

Thank you.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.