Skip to main content
eziya76
Associate III
August 13, 2025
Question

Issue with Programming two MT25QL512ABB devices in dual mode using the STM32H747I

Hello,

I hope this message finds you well. I am currently testing two MT25QL512ABB devices in dual mode using the STMH747I, with the same driver for the MT25QL512ABB. After performing write/read verification and rebooting, I encounter issues during subsequent read operations, as it consistently returns 0xFF. I would greatly appreciate your assistance in sharing any insights or findings regarding the root cause of this issue, if available. Thank you in advance for your support.

Edit: moved from Issue with Programming NOR Flash MT25QL512ABB1EW9 Using STM32H735IGT6 to a new thread.

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
August 20, 2025

Hello,

 

Same issue is reported here.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.