Skip to main content
phenom
Associate III
November 29, 2019
Question

Implement UART Transmit in DMA mode correct way

I am using stm32f779I eval kit. I am using example UART_HyperTerminal_DMA by en.stm32cubef7.

I am trying to implement UART in DMA mode to transmit a simple string.

So I have used CubeMX to generate the code and I have configured UART1 TX DMA in normal mode.

Whenever I run the code in debugging mode, I see the first time I attemp to send the string, it works ok and sends the string.

But I couldn't send a second transmission.

Can any one please suggest the correct way to use Uart Tx in DMA mode? How can I send successive strings one after another?

E.g. :

i used

 if(HAL_UART_Transmit_DMA(&UartHandle, (uint8_t*)aTxStartMessage, TXSTARTMESSAGESIZE-10)!= HAL_OK)

 {

  /* Transfer error in transmission process */

  Error_Handler();

 }

 if(HAL_UART_Transmit_DMA(&UartHandle, (uint8_t*)aTxStartMessage, TXSTARTMESSAGESIZE-10)!= HAL_OK)

 {

  /* Transfer error in transmission process */

  Error_Handler();

 }

2 times HAL_UART_Transmit_DMA() API. 2nd time API has huart->gState == HAL_UART_STATE_BUSY_TX

This topic has been closed for replies.

14 replies

Jame DEV
Associate II
November 29, 2019

Check this one.

https://community.st.com/s/question/0D50X0000BcPXk2SQG/32f746-usart-dma-with-stemwin-not-working

and maybe you forget to wait for uart DMA working. If uart DMA is not finished the first message. the huart is in busy state so the second message will not work. try add this code before next transmit.

 while (HAL_UART_GetState(&UartHandle) != HAL_UART_STATE_READY)

 {

 }

phenom
phenomAuthor
Associate III
November 29, 2019

Hi,

I have added code as suggested by you:

Print()

{

HAL_UART_Transmit_DMA(&UartHandle, (uint8_t *)ch, len);

  while (HAL_UART_GetState(&UartHandle) != HAL_UART_STATE_READY)

  {

  }

}

 But after HAL_UART_Transmit_DMA() execution pointer goes to

 void DMA2_Stream7_IRQHandler(void)

{

  HAL_DMA_IRQHandler(UartHandle.hdmatx);

};

in stm32f7xx_it.c and then comes back to 

  while (HAL_UART_GetState(&UartHandle) != HAL_UART_STATE_READY)

  {

  }

Here while loop never ends.

Jame DEV
Associate II
November 29, 2019

Did you check the first signal transmission . Do it have data output? if it's not.

Please check MX_DMA_Init() function. you have to call this function before MX_USARTx_UART_Init().

phenom
phenomAuthor
Associate III
November 29, 2019

My issue is same as

https://community.st.com/s/question/0D50X00009XkgtY/dma-uart-with-hal-remain-busy-bug

but solution provided in this link is not working for me.

Already  HAL_UART_IRQHandler()  enabled.

waclawek.jan
Super User
November 30, 2019

Do you observe the Tx pin using an oscilloscope/LA? Is there any activity related to the second "batch" of data?

Read out and check the USART and relevant DMA registers content.

JW

phenom
phenomAuthor
Associate III
December 2, 2019

Hi,

I have added code as suggested by you:

Print()

{

HAL_UART_Transmit_DMA(&UartHandle, (uint8_t *)ch, len);

  while (HAL_UART_GetState(&UartHandle) != HAL_UART_STATE_READY)

  {

  }

}

 But after HAL_UART_Transmit_DMA() execution pointer goes to

 void DMA2_Stream7_IRQHandler(void)

{

  HAL_DMA_IRQHandler(UartHandle.hdmatx);

};

in stm32f7xx_it.c and then comes back to 

  while (HAL_UART_GetState(&UartHandle) != HAL_UART_STATE_READY)

  {

  }

Here while loop never ends.

KRich.4
Visitor II
February 9, 2022

Hey,

I am facing the same issue. How did you solve it? Thank you for your Answer.

I am using a STM32G4

Visitor II
August 12, 2024

Facing exactly same issue, have you ever find the solution and root cause? DISCOVERY 1 stm32f407 board...

Karl Yamashita
Principal
August 12, 2024

You haven't posted any code so no telling what could be wrong.

See if this helps https://github.com/karlyamashita/Nucleo-G431RB_Three_UART/wiki

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source