Skip to main content
Associate II
August 30, 2025
Question

I can't read sdram framebuffer with LTDC

I am developping STM32F469 with TouchGFX to display with LTDC in RGB888. I can display an image in the internal SRAM. However, when trying with SDRAM, the screen truns black, and the debugger can only read 0s. But when I tried with the framebuffer reader offered by ST, I can still read the image which seems to be already loaded into the SDRAM. Is there any suggestions to figure out the issue to give a final solution?

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
September 1, 2025

Hello @123scy321 and welcome to the community;

 

Could you please check the SDRAM configuration for that you can refer to How to set up the FMC peripheral to interface with the SDRAM IS42S16800F-6BLI from ISSI article.

Also, I recommend you to take a look at AN4861 application note precisely "5.5.2 Optimizing the LTDC framebuffer fetching from external memories (SDRAM or SRAM)" and "5.5.3 Optimizing the LTDC framebuffer fetching from SDRAM" sections.

 

I hope this help you!

Thank you.

Kaouthar

 

 

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.