Skip to main content
Associate II
Feb 18, 2025 8:37 AM UTC
Solved

How to control STM32H7RS GPIO port P and N?

I use NUCLEO-H7S3L8 to evaluate our new solution. I want to use GPIO port P to control a few external components.

I add some test code into NUCLEO-H7S3L8\Examples\GPIO\GPIO_IOTggle project, like the below snapped code:

__HAL_RCC_GPIOP_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOP, &GPIO_InitStruct);
HAL_GPIO_WritePin(GPIOP, GPIO_PIN_0, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOP, GPIO_PIN_1, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOP, GPIO_PIN_2, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOP, GPIO_PIN_3, GPIO_PIN_SET);

After executed the above code, I halted the core and measured voltage of these pins with a multi-meter.

These pins keep LOW voltage.

Does it need an additional configuration when we want to use GPIO port M to P in STM32H7RS?


Code formatting applied - please see How to insert source code for future reference.

This topic has been closed for replies.
Tony2SimmyBest answer
Associate II
Mar 5, 2025 7:30 AM UTC

Need to enable a special power domain. You' better to use CUBE to generate sample code.

8 replies

Andrew Neil
Super User
Feb 18, 2025 8:52 AM UTC

Have you checked that the Nucleo board doesn't have anything else connected to those pins?

Check the User Manual and/or schematics ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
Feb 18, 2025 9:04 AM UTC

Hi Andrew, thank for your reply.

I had checked the schematic, those pins connect to a connector.

Actually i had tested port N which have test points in other project, results is same.

Tony2SimmyAuthorBest answer
Associate II
Mar 5, 2025 7:30 AM UTC

Need to enable a special power domain. You' better to use CUBE to generate sample code.

Andrew Neil
Super User
Mar 5, 2025 8:09 AM UTC

Has that solved your issue?

If so, please mark that as the solution:

https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.