Skip to main content
Associate
May 19, 2026 7:18 AM UTC
Question

High-Speed Data Logging Architecture: 10MSPS Interleaved ADC to eMMC + USB on STM32H743

Hello,

I am designing a high-speed data logging architecture using STM32H743VIHx. I would like the community to validate my DMA architecture and answer specific questions about eMMC access. I did not find answers in the forum and I am also not an expert in microcontroller hardware/software architecture.

 

--- SYSTEM OVERVIEW ---

The logging produces a continuous signal sampled by the ADC. I need to log raw data samples along with GPS and IMU data to an eMMC for post-processing.

Key parameters:
- ADC: 14-bit dual interleaved on PA6 (ADC12_INP3), differential ~10 MSPS effective
- eMMC: S32 GB, eMMC 5.1
- SDMMC1 in 8-bit MMC mode
- IMU: on SPI2 (PB12-15) at 8 kHz
- GPS: on UART4 at 115200 baud

 

--- PROPOSED DMA ARCHITECTURE ---

Four concurrent DMA paths:

1. ADC1+ADC2 interleaved → DMA1_Stream0 → AXI SRAM (ping buffer)
Triggered by ADC1 EOC, reads CDR register (32-bit = 2 interleaved samples)
Rate: ~20 MB/s
Priority: VERY HIGH

2. AXI SRAM (pong buffer) → MDMA_Channel0 → SDMMC1 → eMMC
Triggered after 128 consecutive measurements
Burst write: 2.56 MB per transfer
Rate: ~45 MB/s burst
Priority: HIGH

3. SPI2 → DMA1_Stream4 → AXI SRAM (IMU buffer)
Triggered by IMU INT1 at 8 kHz
Rate: ~1 MB/s
Priority: MEDIUM

4. UART4 → DMA2_Stream2 → AXI SRAM (GPS buffer)
Circular DMA, UART idle detection
Rate: ~14 KB/s
Priority: LOW

Ping-pong buffers in AXI SRAM, 32-byte aligned, DCache cleaned before MDMA read.

 

--- QUESTIONS ---

Q1 - ADC dual interleaved validation
Is PA6 (ADC12_INP3) a valid fast channel for dual interleaved differential mode at 10 MSPS / 14-bit on the STM32H743VIHx ? AN5354 states 10 MSPS at 14-bit is achievable on fast channels but does not list specific pins for the 100-pin package. I have seen a community post confirming ADC12_INP3 (PA6), ADC12_INP4 (PC4), and ADC12_INP5 (PB1) as the only fast channels.

 

Q2 — DMA parallelism
Can DMA1_Stream0 (ADC→SRAM) and MDMA_Channel0 (SRAM→SDMMC) run simultaneously without stalling the ADC path? My AXI SRAM load calculation gives ~66 MB/s total against ~960 MB/s realistic bandwidth — well within limits. However I am concerned about bus arbitration causing microsecond stalls on the ADC DMA during MDMA burst writes. Has anyone experienced ADC sample loss during simultaneous MDMA eMMC writes?

 

Q3 — eMMC offline readout via USB
After the flight I need to read the raw eMMC data on a PC for post-processing.
Can I implement USB MSC using the H743 USB OTG FS on PA11/PA12. The STM32 reads eMMC via SDMMC1 and exposes it as a USB drive. Is it possible ? What component do I need to add ?

 

Q4 — eMMC raw sector access without filesystem
I am writing raw sectors directly (no FatFS) using HAL_MMC_WriteBlocks_DMA for performance. After plugging via USB MSC, will the PC see the device as a raw disk ? Or does USB MSC require the device to have a valid MBR/partition table?

 

Thank you for any feedback. I am really not an expert in this domain and I tried my best to gather informations. But I am not 100% sure of what I found as it is a mix of forums answers, datasheets and Claude AI help.

Florian

9 replies

Ozone
Principal
May 19, 2026 8:02 AM UTC

First, I don't have experience with the H7 series as such.

> AN5354 states 10 MSPS at 14-bit is achievable on fast channels but does not list specific pins for the 100-pin package.

This information is found in the datasheet, especially the pinout section with GPIO AF options. I have seen such "fast channel" comments as table footnotes.

> Can DMA1_Stream0 (ADC→SRAM) and MDMA_Channel0 (SRAM→SDMMC) run simultaneously without stalling the ADC path?

Things get a bit more complex here.
Check the reference manual sections describing the bus matrix, and the corresponding sections for the involved peripherals. DMA transfers and core data memory accesses can indeed interfer with each other if they use the same bus.

> The STM32 reads eMMC via SDMMC1 and exposes it as a USB drive. Is it possible ? What component do I need to add ?

Definitely possible.
You could check for an USB MSC example for your MCU, build and test it, and integrate it into your application.

> I am writing raw sectors directly (no FatFS) using HAL_MMC_WriteBlocks_DMA for performance. After plugging via USB MSC, will the PC see the device as a raw disk ? Or does USB MSC require the device to have a valid MBR/partition table?

Not sure what you mean.
If you speak about using the H7 as USB-MSC device, the internal organisation of the eMMC memory does not really matter in this case.
But you need to present it to the host system (the PC) as a file system it understands - e.g. FAT32.

ST Technical Moderator
May 19, 2026 9:16 AM UTC

Hi  @Krawyn 

  1. I assume already answered here as well.
  2. Even if your AXI SRAM bandwidth calculation is well within limits, bus arbitration can introduce µs stalls. These stalls, especially during MDMA burst writes, can cause ADC sample loss or overruns in similar scenarios. This is due to the way STM32 bus matrices handle multiple masters competing for the same memory resources. Arbitration delays can occur, particularly if both DMA and MDMA target the same SRAM region at the same time. To minimize this risk, use staged transfers, synchronize operations with callbacks, assign higher priority to ADC DMA if needed, and balance memory accesses. 
  3. Check this example application article for implementing a standalone USB Mass Storage device on STM32 with eMMC. It could be useful in your case.
  4. Regarding USB MSC device, USB Mass Storage Class exposes a block device, so a PC can access sectors directly. However, for the PC to automatically mount and use the storage as a normal disk, a valid partition table and usually a valid filesystem are expected. So,
  • Raw sector access is possible
  • USB MSC device does not inherently require a filesystem
  • But without a valid MBR/GPT and filesystem, the PC may detect the media as a raw/unformatted disk rather than a usable volume.
To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
KrawynAuthor
Associate
May 20, 2026 7:49 AM UTC

Hello @FBL ,

Thank you for the answer.

  1. This post and datasheet speak about single ended ADC if I am not mistaken. Does it apply for differential ADC too ? I don't see a difference in the datasheet but I assume there is one, no ?
  2. Does it mean using different SRAM regions solves this issue ?
  3. This example uses USB_OTG_FS. I found code examples for USB_OTG_HS which is required in my case (6-10Gb of data to transfer). I was wondering if I need to simply add a USB controller between the STM32 and the USB port to support high-speed ? I did not find any example showing high-speed hardware implementation
  4. This is clear for me now. I think Linux can read the file once the storage is mounted if I understood correctly

 

Thank you once again for the help

Ozone
Principal
May 20, 2026 10:58 AM UTC

> This post and datasheet speak about single ended ADC if I am not mistaken. Does it apply for differential ADC too ? I don't see a difference in the datasheet but I assume there is one, no ?

If you speak about internal ADC, surely not. It is just a different configuration, but the data rate remains the same.
This is at least true for other STM32 MCUs with ADCs that support a (pseudo-) differential mode.

> Does it mean using different SRAM regions solves this issue ?
Not necessarily.
Only if different RAM region with connection to different busses are concerned - those could runinparallel without interference. If the transfers need to go through the same internal bus, the addresses do not matter.
I can only refer to the DS / RM documents for details, since I lack the experience with H7 devices.

Ozone
Principal
May 20, 2026 6:08 AM UTC

> The logging produces a continuous signal sampled by the ADC. I need to log raw data samples along with GPS and IMU data to an eMMC for post-processing.

> Key parameters:
> - ADC: 14-bit dual interleaved on PA6 (ADC12_INP3), differential ~10 MSPS effective
> ...

If I might ask, what do you need the full analog input bandwidth for in the logs (ADC @10Msps = 20MB/s) ?
The project seems to involve an autonomous drone, or a similiar flying/moving object.

However, whatever this ADC channel measures, it most probably is only important when the values are incorporated with IMU and GPS data into some state vector, which happens at a much lower rate.

I would consider logging filtered / transposed ADC values instead, perhaps validating the processing of this analog value separately.
This would significantly ease the requirement.

KrawynAuthor
Associate
May 20, 2026 7:54 AM UTC

Hello @Ozone 

Thank you for the interest. It is a student project for radar thus the requirement of full bandwidth for FFT post-processing. I indeed need precise position hence the GPS and IMU. The ADC values needs to be aligned with correct position as you understood. I planned to have a block of GPS+IMU (low rate sampling) then a big block of ADC data (higher sampling rate). 

  • ADC data every 10MSPS
  • GPS and IMU present every 1Hz-10Hz

 

This was my implementation idea. If you have a better idea, I would be very interested into hearing it. I did not fully understood what you meant by logging filtered ADC values to reduce the sampling rate

 

Sincerely

Ozone
Principal
May 20, 2026 8:24 AM UTC

> It is a student project for radar thus the requirement of full bandwidth for FFT post-processing.

I think this "FFT post-processing path" can be easily validated separately.

You could use a single-shot method, i.e. log one or FFT-sized blocks of ADC data to RAM, perhaps including FFT / post-processing results, and transfer them to a host offline.
You can thus check and validate this post-processing separately, until the results satisfy expectations.

For the mentioned system log, you could store the result of this post-processing instead of raw ADC data, probably some estimated object coordinates. I suppose this results consume much less space, and would significantly reduce eMMC throughput and possible system congestion issues.

ST Technical Moderator
May 20, 2026 10:45 AM UTC

Hi @Krawyn 

>This post and datasheet speak about single ended ADC if I am not mistaken. Does it apply for differential ADC too ? I don't see a difference in the datasheet but I assume there is one, no ?

Yess

>Does it mean using different SRAM regions solves this issue ?

I don't get your point here.

> I did not find any example showing high-speed hardware implementation

You can refer to MB1246

FBL_0-1779273813974.png

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
LCE
Principal III
May 20, 2026 12:53 PM UTC

I would indeed make use of DTCM and ITCM RAM of the H7 as much as possible.

With these data rates and basically constant DMA use of the bus, try to keep almost everything else out of the AXI RAM.

DTCM: use for all variables except buffers for DMA (DMA cannot access TSM RAM anyway *)

ITCM: can be used for interrupt handlers (also heap and stack *)

 

* at least in the H723..H735 that I use

 

Anyway, this is quite a project for a beginner! Expect failure and lots of teeth grinding... ;)