Skip to main content
Associate
Jan 12, 2026 3:43 AM UTC
Solved

HAL_CAN_START returns 131072

Hi. I'm new to STM32, and I'm using STM32F103C8T6. I want to run Loopback mode to test CAN BUS without another board first. When I go to debug, I find it stuck at HAL_CAN_START. It returns error code 131072. Can you guys please help me find out the problem? I also give the main.c below. Thanks for reading.

/* USER CODE BEGIN Header */

/**

******************************************************************************

* @file : main.c

* @brief : Main program body

******************************************************************************

* @attention

*

* Copyright (c) 2026 STMicroelectronics.

* All rights reserved.

*

* This software is licensed under terms that can be found in the LICENSE file

* in the root directory of this software component.

* If no LICENSE file comes with this software, it is provided AS-IS.

*

******************************************************************************

*/

/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/

#include "main.h"

 

/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */

 

/* USER CODE END Includes */

 

/* Private typedef -----------------------------------------------------------*/

/* USER CODE BEGIN PTD */

 

/* USER CODE END PTD */

 

/* Private define ------------------------------------------------------------*/

/* USER CODE BEGIN PD */

 

/* USER CODE END PD */

 

/* Private macro -------------------------------------------------------------*/

/* USER CODE BEGIN PM */

 

/* USER CODE END PM */

 

/* Private variables ---------------------------------------------------------*/

CAN_HandleTypeDef hcan;

 

/* USER CODE BEGIN PV */

 

/* USER CODE END PV */

 

/* Private function prototypes -----------------------------------------------*/

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_CAN_Init(void);

/* USER CODE BEGIN PFP */

 

/* USER CODE END PFP */

 

/* Private user code ---------------------------------------------------------*/

/* USER CODE BEGIN 0 */

 

CAN_TxHeaderTypeDef TxHeader;

CAN_RxHeaderTypeDef RxHeader;

 

uint8_t TxData[8];

uint8_t RxData[8];

 

uint32_t TxMailbox;

 

uint8_t count = 0;

 

void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)

{

HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &RxHeader, RxData);

count++;

}

/* USER CODE END 0 */

 

/**

* @brief The application entry point.

* @retval int

*/

int main(void)

{

 

/* USER CODE BEGIN 1 */

 

/* USER CODE END 1 */

 

/* MCU Configuration--------------------------------------------------------*/

 

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */

HAL_Init();

 

/* USER CODE BEGIN Init */

 

/* USER CODE END Init */

 

/* Configure the system clock */

SystemClock_Config();

 

/* USER CODE BEGIN SysInit */

 

/* USER CODE END SysInit */

 

/* Initialize all configured peripherals */

MX_GPIO_Init();

MX_CAN_Init();

/* USER CODE BEGIN 2 */

 

if (HAL_CAN_Start(&hcan) != HAL_OK) Error_Handler();

if (HAL_CAN_ActivateNotification(&hcan, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK) Error_Handler();

 

TxHeader.DLC = 1;

TxHeader.IDE = CAN_ID_STD;

TxHeader.RTR = CAN_RTR_DATA;

TxHeader.StdId = 0x103;

 

TxData[0] = 0x15;

 

if (HAL_CAN_AddTxMessage(&hcan, &TxHeader, TxData, &TxMailbox) != HAL_OK) Error_Handler();

 

/* USER CODE END 2 */

 

/* Infinite loop */

/* USER CODE BEGIN WHILE */

while (1)

{

/* USER CODE END WHILE */

 

/* USER CODE BEGIN 3 */

}

/* USER CODE END 3 */

}

 

/**

* @brief System Clock Configuration

* @retval None

*/

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct = {0};

RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 

/** Initializes the RCC Oscillators according to the specified parameters

* in the RCC_OscInitTypeDef structure.

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

RCC_OscInitStruct.HSEState = RCC_HSE_ON;

RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler();

}

 

/** Initializes the CPU, AHB and APB buses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)

{

Error_Handler();

}

}

 

/**

* @brief CAN Initialization Function

* @param None

* @retval None

*/

static void MX_CAN_Init(void)

{

 

/* USER CODE BEGIN CAN_Init 0 */

 

/* USER CODE END CAN_Init 0 */

 

/* USER CODE BEGIN CAN_Init 1 */

 

/* USER CODE END CAN_Init 1 */

hcan.Instance = CAN1;

hcan.Init.Prescaler = 18;

hcan.Init.Mode = CAN_MODE_LOOPBACK;

hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;

hcan.Init.TimeSeg1 = CAN_BS1_2TQ;

hcan.Init.TimeSeg2 = CAN_BS2_1TQ;

hcan.Init.TimeTriggeredMode = DISABLE;

hcan.Init.AutoBusOff = DISABLE;

hcan.Init.AutoWakeUp = DISABLE;

hcan.Init.AutoRetransmission = DISABLE;

hcan.Init.ReceiveFifoLocked = DISABLE;

hcan.Init.TransmitFifoPriority = DISABLE;

if (HAL_CAN_Init(&hcan) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN CAN_Init 2 */

 

CAN_FilterTypeDef canfilterconfig;

 

canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;

canfilterconfig.FilterBank = 0; // which filter bank to use from the assigned ones

canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO0;

canfilterconfig.FilterIdHigh = 0;

canfilterconfig.FilterIdLow = 0x0000;

canfilterconfig.FilterMaskIdHigh = 0;

canfilterconfig.FilterMaskIdLow = 0x0000;

canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;

canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;

canfilterconfig.SlaveStartFilterBank = 14; // how many filters to assign to the CAN1 (master can)

 

if (HAL_CAN_ConfigFilter(&hcan, &canfilterconfig) != HAL_OK) Error_Handler();

 

/* USER CODE END CAN_Init 2 */

 

}

 

/**

* @brief GPIO Initialization Function

* @param None

* @retval None

*/

static void MX_GPIO_Init(void)

{

/* USER CODE BEGIN MX_GPIO_Init_1 */

 

/* USER CODE END MX_GPIO_Init_1 */

 

/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOD_CLK_ENABLE();

__HAL_RCC_GPIOA_CLK_ENABLE();

__HAL_RCC_GPIOB_CLK_ENABLE();

 

/* USER CODE BEGIN MX_GPIO_Init_2 */

 

/* USER CODE END MX_GPIO_Init_2 */

}

 

/* USER CODE BEGIN 4 */

 

/* USER CODE END 4 */

 

/**

* @brief This function is executed in case of error occurrence.

* @retval None

*/

void Error_Handler(void)

{

/* USER CODE BEGIN Error_Handler_Debug */

/* User can add his own implementation to report the HAL error return state */

__disable_irq();

while (1)

{

}

/* USER CODE END Error_Handler_Debug */

}

#ifdef USE_FULL_ASSERT

/**

* @brief Reports the name of the source file and the source line number

* where the assert_param error has occurred.

* @param file: pointer to the source file name

* @param line: assert_param error line source number

* @retval None

*/

void assert_failed(uint8_t *file, uint32_t line)

{

/* USER CODE BEGIN 6 */

/* User can add his own implementation to report the file name and line number,

ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

/* USER CODE END 6 */

}

#endif /* USE_FULL_ASSERT */

 

 

 

Dang_VAA_0-1768189276590.png

 

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 12, 2026 9:33 AM UTC

@Dang_VAA wrote:

I'm pretty sure that I remapped the pins and set bit time segments as you advised. 


Based on your first statement: "PB8 and PB9 are used for CAN_RX and CAN_TX pins. When I use PA11 and PA12, it's still OK. But when remapping to PB8 and PB9 with the same code, it gets stuck"

I'm almost sure that's a hardware issue. As I don't have all the hardware elements nor the schematic details, I cannot help you at this stage.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

13 replies

mƎALLEm
ST Technical Moderator
Jan 12, 2026 8:06 AM UTC

Hello @Dang_VAA and welcome to the ST community,

What board are you using? Blue Pill?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Dang_VAAAuthor
Associate
Jan 12, 2026 8:40 AM UTC

Yes. It's not actually a Blue Pill. But that kit uses the same chip (STM32F103C8T6) as Blue Bill. The kit includes transceiver A1050. PB8 and PB9 are used for CAN_RX and CAN_TX pins. When I use PA11 and PA12, it's still OK. But when remapping to PB8 and PB9 with the same code, it gets stuck, as I said.

mƎALLEm
ST Technical Moderator
Jan 12, 2026 8:50 AM UTC

In next time please use </> button to share your code:

mALLEm_0-1768207580723.png

1- Did you modify the hardware on the board to connect the new CAN pins to the transceiver? if yes how you did that?

2- Share the schematics of the board and tell what you have modified on it?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Dang_VAAAuthor
Associate
Jan 12, 2026 9:08 AM UTC

1. First, I use STM32CubeMX to modify CAN pins. I activate CAN, then remap at Pinout View.
2. The kit I borrowed from my mate. And I have searched the web for the schematic, but none match that kit.
I use VOM to find out where the TX and RX on the transceiver are connected to.

Dang_VAA_0-1768208924266.jpeg

 

mƎALLEm
ST Technical Moderator
Jan 12, 2026 8:54 AM UTC

+

These are bad CAN bit timing parameters:

hcan.Init.Prescaler = 18;
hcan.Init.Mode = CAN_MODE_LOOPBACK;
hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan.Init.TimeSeg1 = CAN_BS1_2TQ;
hcan.Init.TimeSeg2 = CAN_BS2_1TQ;

Avoid using 1TQ to set one of the bit time segments.

Please read this article: CAN (bxCAN) bit time configuration on STM32 MCUs :

mALLEm_0-1768208139151.png

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Dang_VAAAuthor
Associate
Jan 12, 2026 9:11 AM UTC

Ok. Thanks for pointing out my fault. I changed that too. Now, how can I find out what my problem is?