Question
H7 read temperature from ADC
H friends,
I'm trying to read adc3, a temperature sensor from stm32h753. But something is wrong. Because I didn't get any interruptions. Can anyone help?
void MX_ADC3_Init(void) {
LL_RCC_SetADCClockSource(LL_RCC_ADC_CLKSOURCE_CLKP);
/* Peripheral clock enable */
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_ADC3);
if (LL_ADC_IsDeepPowerDownEnabled(ADC3) != 0UL)
LL_ADC_DisableDeepPowerDown(ADC3);
if (LL_ADC_IsInternalRegulatorEnabled(ADC3) == 0UL) {
LL_ADC_EnableInternalRegulator(ADC3);
__IO uint32_t wait_loop_index = 0UL;
wait_loop_index = ((LL_ADC_DELAY_INTERNAL_REGUL_STAB_US / 10UL) * (SystemCoreClock / (100000UL * 2UL))) + 1000;
while (wait_loop_index != 0UL) {
wait_loop_index--;
}
}
LL_ADC_SetCommonClock(__LL_ADC_COMMON_INSTANCE(ADC3), LL_ADC_CLOCK_ASYNC_DIV2);
LL_ADC_SetResolution(ADC3, LL_ADC_RESOLUTION_16B);
LL_ADC_REG_SetSequencerLength(ADC3, LL_ADC_REG_SEQ_SCAN_ENABLE_10RANKS);
LL_ADC_SetLowPowerMode(ADC3, LL_ADC_LP_MODE_NONE);
LL_ADC_REG_SetContinuousMode(ADC3, LL_ADC_REG_CONV_CONTINUOUS);
LL_ADC_REG_SetSequencerDiscont(ADC3, LL_ADC_REG_SEQ_DISCONT_DISABLE);
LL_ADC_REG_SetTriggerSource(ADC3, LL_ADC_REG_TRIG_SOFTWARE);
LL_ADC_REG_SetDataTransferMode(ADC3, LL_ADC_REG_DMA_TRANSFER_UNLIMITED);
LL_ADC_REG_SetOverrun(ADC3, LL_ADC_REG_OVR_DATA_OVERWRITTEN);
LL_ADC_SetOverSamplingScope(ADC3, LL_ADC_OVS_DISABLE);
LL_ADC_REG_SetSequencerRanks(ADC3, LL_ADC_REG_RANK_1, LL_ADC_CHANNEL_TEMPSENSOR);
LL_ADC_SetChannelSamplingTime(ADC3, LL_ADC_CHANNEL_TEMPSENSOR, LL_ADC_SAMPLINGTIME_387CYCLES_5);
LL_ADC_SetChannelSingleDiff(ADC3, LL_ADC_CHANNEL_TEMPSENSOR, LL_ADC_SINGLE_ENDED);
LL_ADC_SetOffset(ADC3, LL_ADC_OFFSET_1, LL_ADC_CHANNEL_TEMPSENSOR, 0);
LL_ADC_EnableIT_EOS(ADC3); // End of regular sequence of conversions IR enable
LL_ADC_EnableIT_EOC(ADC3); // End of conversion IR enable
}
void init_DMA_ADC(void) {
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_STREAM_1, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
LL_DMA_DisableFifoMode(DMA1, LL_DMA_STREAM_1);
LL_DMA_SetMemoryBurstxfer(DMA1, LL_DMA_STREAM_1, LL_DMA_MBURST_SINGLE);
LL_DMA_SetMemorySize(DMA1, LL_DMA_STREAM_1, LL_DMA_MDATAALIGN_HALFWORD);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_STREAM_1, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetMode(DMA1, LL_DMA_STREAM_1, LL_DMA_MODE_CIRCULAR);
LL_DMA_SetPeriphBurstxfer(DMA1, LL_DMA_STREAM_1, LL_DMA_PBURST_SINGLE);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_STREAM_1, LL_DMA_PDATAALIGN_HALFWORD);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_STREAM_1, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetPeriphRequest(DMA1, LL_DMA_STREAM_1, LL_DMAMUX1_REQ_ADC3);
LL_DMA_SetStreamPriorityLevel(DMA1, LL_DMA_STREAM_1, LL_DMA_PRIORITY_HIGH);
LL_DMA_SetPeriphAddress(DMA1, LL_DMA_STREAM_1, (uint32_t) (&ADC3->DR));
LL_DMA_SetMemoryAddress(DMA1, LL_DMA_STREAM_1, (uint32_t)tempSensor);
LL_DMA_EnableIT_TC(DMA1, LL_DMA_STREAM_1);
}
void enable_adc_interrupt(void) {
NVIC_SetPriority(ADC3_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
NVIC_EnableIRQ(ADC3_IRQn);
}
void enable_dma_interrupt(void) {
NVIC_SetPriority(DMA1_Stream1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 0, 0));
NVIC_EnableIRQ(DMA1_Stream1_IRQn);
}
void enable_ADC(void)
{
LL_ADC_Enable(ADC3);
while (LL_ADC_IsEnabled(ADC3) == 0UL);
}
void start_ADC(uint32_t size)
{
LL_DMA_SetDataLength(DMA1, LL_DMA_STREAM_1, size);
LL_DMA_EnableStream(DMA1, LL_DMA_STREAM_1);
LL_ADC_REG_StartConversion(ADC3);
}
void DMA1_Stream1_IRQHandler(void) {
if (LL_DMA_IsActiveFlag_TC1(DMA1)) {
LL_DMA_ClearFlag_TC1(DMA1);
dma_flag = 1;
}
}
void ADC3_IRQHandler(void) {
if(LL_ADC_IsActiveFlag_EOC(ADC3) || LL_ADC_IsActiveFlag_EOS(ADC3) ){
LL_ADC_ClearFlag_EOC(ADC3);
LL_ADC_ClearFlag_EOS(ADC3);
adc_flag = 1;
}
}i call it in my main:
MX_ADC3_Init();
init_DMA_ADC();
enable_adc_interrupt();
enable_dma_interrupt();
enable_ADC();
start_ADC(2); // 2 for 2x half wordAnd in while ufnction I have condition:
if ((adc_flag == 1) || (dma_flag == 1)){
adc_flag = 0;
dma_flag = 0;
// breakpoint here
}my studing material is datasheet, reference manual and internet...