Skip to main content
hajermarnissi
Associate II
March 21, 2011
Question

FILE AXF

Posted on March 21, 2011 at 13:34

FILE AXF

    This topic has been closed for replies.

    12 replies

    hajermarnissi
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 14:29

    Hello

    Sorry

    ,

     

    I did not

     

    understand

     

    that

     

    I must do clive1

    .

    Thank you

    Rosa

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:29

    If you are unable to use the tools or make this determination, you should probably call Keil technical support and work through it with them.

    You should be able to compile/debug directly into the board via JTAG if you have the project/memory set up correctly. The AXF file contains a lot more information beyond the executable code. If you download the AXF directly into the STM32's memory space you might well have a problem as it is not native binary.

    I wish you'd stick to one thread rather than opening a new one every time you have a thought.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:29

    Sounds like you need to get a properly licensed version of Keil to work on an application of that size.

    How are you writing the AXF to the part?

    Can you generate a BIN or HEX file and program that with J-Flash or ST-LINK?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 14:29

    ''you

     

    know

     

    where

     

    the

     

    problem?''

    It seems to me that the problem is that you are trying to run a marathon before learning to crawl - let alone walk.

    Do you have any prior programming experience in general?

    Do you have any prior programming experience with small embedded microcontrollers in particular?

     

     

    Have you taken any time to study the Keil documentation, and familiarise yourself with the tools and their use?

    Have you taken any time to study the GUI library documentation, examples, etc, and familiarise yourself with the tools and their use?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    hajermarnissi
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 14:29

    Hello

    Since

     

    I

     

    can

     

    not

     

    on

     

    Keil

     

    debugging purposes

     

    must

     

    simulate

     

    directly

     

    on

     

    the target

    because

     

    the

     

    maximum file size

     

    for debugging

     

    on

     

    Keil

     

    is

     

    32KB

     

    by

     

    my

     file size is 

    941Ko

    , you

     

    know

     

    where

     

    the

     

    problem

    Thank you

    hajermarnissi
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 14:29

    Hello neil.andrew

    We can

     

    say that

     

    I mastered

     

    the

     

    programming,

     

    graphics

     

    library

    ,

     

    user

     

    manual 

    touchscreen

     

    with

     

    this library

    I

     

    said

     

    the

     

    simulation

    , ie

     

    testing

     

    the

     

    program on

     

    the

     

    target board

    Thank you

    Rosa

    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 14:29

    ''... simulate

     (sic)

    directly

     

    on

     

    the target...''

     

    If your're running the actual code on the actual target, then that's not simulating - is it?!

    That's the Real Thing - not a simulation!
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    hajermarnissi
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 14:29

    I did not

     

    understand

     

    ''

    my

     

    messages

     

    give

     

    a

     

    very

     

    different

     

    impression

    ''

    Andrew Neil
    Super User
    May 17, 2011
    Posted on May 17, 2011 at 14:29

    ''We can say that I mastered the programming, graphics library, user manual touchscreen with this library''

     

    We could say it - but your posts give a very different impression!

    ''I said the simulation, ie testing the program on the target board''

     

    No, that is not simulation.

    Simulation refers to something that is not the real thing

    http://dictionary.cambridge.org/dictionary/british/simulation

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    raptorhal2
    Lead
    May 17, 2011
    Posted on May 17, 2011 at 14:29

    Your Keil IDE probably has an option to generate a map file. This is a text file with usually a .map extension that can be viewed with the IDE editor. It identifies how much RAM and flash your code requires and is therefore much more useful than the size of an AXF file. Compare the .map information with the processor's 64KB of RAM and 256 KB of flash.

    The Keil IDE in simulation mode executes your code entirely within the PC. Special software included with the IDE replaces target hardware with software functions. When you download your code into the EVAL board or any other processor, you are in target mode where your code is interacting with real, not simulated hardware.

    All of this information is available in the materials provided with the EVAL board and Keil IDE. If you are have a language problem, get someone to help you.

    Cheers, Hal