Skip to main content
Visitor II
Nov 28, 2023 7:28 AM UTC
Solved

FATfs code for stm32f769NIH6

Hi,

Can you priovide any reference SD card fatfs code for stm32f769NIH6 Microcontroller.

Thanks & Regards,

Mounika

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Nov 28, 2023 7:38 AM UTC

Hello @mounika and welcome to the Community :),

The FatFs_uSD example is available in STM32CubeF7 package.

This application provides a description on how to use STM32Cube™ firmware with FatFs middleware component as a generic FAT file system module using STM32F769I-EVAL. The objective is to develop an application making the most of the features offered by FatFs to configure a microSD drive.

I think also this article: How do I Create a File System on a SD card using STM32CubeIDE? can help you.

Thank you.

Kaouthar

 

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

2 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Nov 28, 2023 7:38 AM UTC

Hello @mounika and welcome to the Community :),

The FatFs_uSD example is available in STM32CubeF7 package.

This application provides a description on how to use STM32Cube™ firmware with FatFs middleware component as a generic FAT file system module using STM32F769I-EVAL. The objective is to develop an application making the most of the features offered by FatFs to configure a microSD drive.

I think also this article: How do I Create a File System on a SD card using STM32CubeIDE? can help you.

Thank you.

Kaouthar

 

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
Nov 28, 2023 1:30 PM UTC
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.