Skip to main content
Associate II
September 15, 2025
Question

Fast communication between two STM32U5G9s

Hello, I found in the documentation search for STM32U5G9 that some interfaces available for high-speed communication, such as OctoSPI and HexaSPI, do not seem to support slave mode.

The device we are making requires two STM32U5G9 chips, each connected to a display, and these displays need to show synchronized content. Additionally, one of the U5G9s will connect to a CYW55513IUBGT for network/Bluetooth communication, while the other needs to acquire data through high-speed communication between chips, so UART may not meet the requirements.

Therefore, I would like to understand how I can enable high-speed communication between the two STM32U5G9 chips. ...

This topic has been closed for replies.

10 replies

AScha.3
Super User
September 15, 2025

Hi,

how big is distance between chips ?  (because hi-speed and more than few centimeters...difficult)

Maybe SPI full duplex (up to 80 Mbit, afaik, see ds) might be the way .

If you feel a post has answered your question, please click on " Best Answer ".
Smith_023Author
Associate II
September 15, 2025

Hello, the distance between the chips can reach about 10 cm. Thank you for your suggestion; I haven't tried running SPI at 80 Mbit speed before, but I will give it a try.

MM..1
Super User
September 15, 2025

Hi Agent Smith ... you omit info about how much data ? Try start reading Parallel synchronous transmission using GPIO and DMA or too USB HS is for U5. 

Andrew Neil
Super User
September 15, 2025

So what, exactly, do you mean by "high-speed" communication?

  • How fast ?
  • How much data ?
  • How far ?
  • How often ?
  • etc, etc, ... ?

Does it have to be an STM32U5G9 ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Smith_023Author
Associate II
September 15, 2025

Hello, I apologize for not providing a detailed explanation of what “high speed” means.
I aim to achieve speeds exceeding 10MB/s because I'm developing a low-power, lightweight XR-class device. Significant display discrepancies between the two chips could cause discomfort. Additionally, due to limited ports (DCMI consumes a significant number), the current plan involves one chip handling the EMMC while the other manages the CYW55513IUBGT for network communication. Therefore, this channel must also transfer data received from the network to the EMMC. Communication between chips will be frequent, primarily for display synchronization calibration and data transfer. Regarding the necessity of using the STM32U5G9, it currently appears essential, as only this chip meets the requirements for low power consumption, robust display performance, and extremely compact size.

Andrew Neil
Super User
September 15, 2025

@Smith_023 wrote:

I aim to achieve speeds exceeding 10MB/s .


Is that bit per second, or bytes per second?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
KDJEM.1
ST Technical Moderator
September 15, 2025

Hello @Smith_023 ;

 

The OCTOSPI and HSPI interfaces are designed to operate in master mode only and do not support a master-slave configuration. 

To enable high-speed communication between two STM32U5G9 chips, you cannot use OctoSPI or HexaSPI. Perhaps you can use SPI.

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
September 15, 2025

@KDJEM.1 wrote:

To enable high-speed communication between two STM32U5G9 chips, you cannot use OctoSPI or HexaSPI.


Unless you use a dual-port RAM ... ?

AndrewNeil_0-1757928400342.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
KDJEM.1
ST Technical Moderator
September 15, 2025

Hello;

 

As mentioned in this FAQ, the QUADSPI/OCTOSPI/HSPI/XSPI interfaces work only as masters. The interfaces do not support full duplex. Therefore, it cannot send and receive data simultaneously.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.