Skip to main content
Associate II
June 24, 2024
Solved

External RAM for FrameBuffer on STM32H7S7L8

Good morning to all,
I’d like to ask your advice.
I have to insert an external RAM for the framebuffer because the internal one is not enough for LCD that I will drive (LCD-TFT LVDS 7 inch 1024x600).
Which external RAM do you recommend? Could a QuadSPI work?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
June 24, 2024

Hello,

You can use HSPI interface. You can refer to the STM32H7S78-DK board as reference (using APS256XXN-OBR memory):

SofLit_0-1719239743231.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

6 replies

Leo99Author
Associate II
June 24, 2024

I add that I have a micro LQFP176 pin.
Do I have to use the FMC? Quad or Octo SPI?

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
June 24, 2024

Hello,

You can use HSPI interface. You can refer to the STM32H7S78-DK board as reference (using APS256XXN-OBR memory):

SofLit_0-1719239743231.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Leo99Author
Associate II
June 24, 2024

Thank you! 
The problem is that in the package LQFP that I’m using it is not available the HexaSPI only Octa.

BarryWhit
Lead
June 27, 2024
"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."