Skip to main content
Associate III
May 19, 2026 6:22 AM UTC
Solved

external memory selection for STM32H745 ?


Hi Team,

I am working on board design using STM32H745 (LQFP176 package), and I would like to confirm the correct external memory selection for my smart kitchen application.

Application details:
- MCU: STM32H745 (dual core)
- Package: LQFP176
- USB OTG FS used as HOST to interface a USB camera
- Camera usage: Snapshot (JPEG only, no continuous video streaming)
- Current: 2MP
- Future plan: up to 5MP snapshot
- Additional peripherals:
- I2S (audio codec interface)
- 4× I2C buses
- UART / RS485
- 2× SPI 

For external memory, can I use QSPI PSRAM (APS6404L 8MB), or should I use SDRAM via FMC?


 Please advise which memory type is recommended.  Any guidance or recommended reference designs would be helpful.

 

Thanks
Sathiya

 

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
May 19, 2026 7:56 AM UTC

Hello @Sakthi_IND;

 

To check if the memory is supported with QUADSPI interface, I recommend you to look at Overall FAQs for QUADSPI/OCTOSPI/HSPI/XSPI - STMicroelectronics Community precisely "1.1 How to check whether a device is supported" 

 

Also you can find some example in this article some examples of memories used in ST official boards for STM32.

For hardware recommendations, I advise you to refer 6L2S_Outjob schematic and Getting started with STM32H74xI/G and STM32H75xI/G MCU hardware development - Application note

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

2 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
May 19, 2026 7:56 AM UTC

Hello @Sakthi_IND;

 

To check if the memory is supported with QUADSPI interface, I recommend you to look at Overall FAQs for QUADSPI/OCTOSPI/HSPI/XSPI - STMicroelectronics Community precisely "1.1 How to check whether a device is supported" 

 

Also you can find some example in this article some examples of memories used in ST official boards for STM32.

For hardware recommendations, I advise you to refer 6L2S_Outjob schematic and Getting started with STM32H74xI/G and STM32H75xI/G MCU hardware development - Application note

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
May 19, 2026 8:09 AM UTC

Hello @Sakthi_IND ,

Could you please clarify what relation between the title "Smart kitchen" and the content of your post?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.