Skip to main content
This topic has been closed for replies.

10 replies

BarryWhit
Lead
Jun 24, 2024 12:21 PM UTC

How can you build a bridge out of solder?!? don't be silly. Not enough tensile strength. :thinking_face:

"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."
waclawek.jan
Super User
Jun 24, 2024 2:33 PM UTC

> Perhaps this is something that needs to be explicitly explained & illustrated?

I don't think so.

I'm afraid the users you're referring to did not take the pain to open the respective manual and read it. What are the chances they would read yet another document?

JW

 

Andrew Neil
Super User
Jun 24, 2024 3:06 PM UTC

Not a separate document - it should be in the same document.

But, if they haven't even opened that document ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Sep 24, 2024 3:44 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Oct 10, 2024 5:01 PM UTC

Another one today:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/stm32l552-nucleo-board-hse-error/m-p/729990/highlight/true#M21883

 

As these processors get more and more complex, it becomes more likely that they will be programmed by "pure software" people - who are less likely to be familiar with these hardware details.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Oct 29, 2024 9:38 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
waclawek.jan
Super User
Oct 29, 2024 9:54 AM UTC

We could perhaps concoct some FAQ. Several related Q come into mind, such as

- where's the documentation

- where's the schematics

- where is example code

- where is the original binary which came preprogrammed

- why some pins don't work (because they are connected to on-board resources).

together with some historical-contextual remarks.

JW

 

Andrew Neil
Super User
Oct 29, 2024 10:04 AM UTC

@waclawek.jan wrote:

We could perhaps concoct some FAQ.

 


aka "Knowledge base" articles?

eg, "Solder Bridges: What They Are and How To Use Them"

I made a start here (focussing on the "what"):

https://community.st.com/t5/stm32-mcus-products/to-determine-the-component-of-quot-sb1-quot-in-stm32f407g-disc1/m-p/736824/highlight/true#M264800 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
waclawek.jan
Super User
Oct 29, 2024 2:08 PM UTC

Nice, but I'm not sure newcomers these days have the attention span to follow that. And that's a single A to a single Q... I was thinking about a "I've bought a devboard now what" or even "I want to buy a devboard, any recommendations?" one.

> In some cases, rather than just use a "blob" of solder, a zero-ohm resistor (aka "zero-ohm link") will be fitted:

I wouldn't say "in some cases". It's actually hard to mass-manufacture a solder blob, so IMO all ST boards have 0Ohm resistors (often unmarked) on the factory-closed SBs; but it's okay to use solder blob when the user wants to close them (in other words, users don't need to be intimidated by the 0Ohm resistors, they are OK but not necessary).

JW

Andrew Neil
Super User
Jan 20, 2025 9:33 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.