Skip to main content
Mr_M_from_G
Senior II
Aug 20, 2019 7:20 AM UTC
Solved

differences between STM32H7 rev V and rev Y

Hello,

we use STM32H7 in our new development. I was excited about the announcement of the new revision V because it promises an increase of speed from 400MHz to 480 MHz. My distributor told me that except for that, the devices were hard- and software compatible.

Now I set a rev V STM32H742 into our prototype and after hours found out that there are a number of differences in ADC alone.

  • So my first general question is, if there is a paper summarizing all the differences?
  • My second question is, if the new ADC will in any case have at least the same performance as the old one (we use it at the edge of the old specs)?
  • The third question is, when will a new package for CubeMX be available that support the new revision? I have STM32H7 package ver 1.2.0 and it complains when I try to set sysclk to 480 MHz.

Now some questions in detail:

  • There is a new clk divider by two for adc_ker_clk. With the old settings for rev Y I get only half the samples per second. Can I simply double pll2_p_ck to get back to the old samples per second or are there limits in the ADC peripheral. (I tried it and it works but I need to be sure, that it is within specs)
  • Datasheet of rev V gives for 14 bits resolution only 3.3 MSps which is too little for us. But it also says that this is with SMP = 2.5 while it is also possible to set SMP = 1.5, which is the value used in rev Y specs for all resolutions. Is there something wrong with using SMP = 1.5 with 14 bit resolution (or any other resolution) for rev V ?
  • Is it still true, that fast channels are channels 0 .. 5 (RM0433 Rev 6 page 910)? Datasheet of STM32H742 says: (page 283) "4. Fast channels correspond to PC0, PC1, PC2, PC3, PA0, and PA1". We use PA6/7 = ADC1 INx3 and PC4/5 = ADC2 INx4 which would be fast for RM0433 but not for the datasheet.

I think we really need solutions for that because we can't stick to rev Y, it will not be produced anymore I guess (??)

So any help especially from ST members is greatly welcome

Thanks a lot

Martin

This topic has been closed for replies.
roland van straten
Associate III
Aug 23, 2019 8:24 AM UTC

I have some documents that explain the die change. One of them is AN5312 which describes the changes and ES0392 describing the errata. I received this some time ago from my distributer as I also use the H743.

You can find them through searching the ST.com website.

12 replies

Rob vdH
Associate
Aug 19, 2020 1:46 PM UTC

Investigated the strange /2 ADC clock divider a bit further and inside the ADC_ConfigureBoostMode function I came across the following code:

else /* STM32H7 silicon Rev.V */
 {
 freq /= 2U; /* divider by 2 for Rev.V */
 
 if (freq <= 6250000UL)
 {
 MODIFY_REG(hadc->Instance->CR, ADC_CR_BOOST, 0UL);
 }
 else if (freq <= 12500000UL)
 {
 MODIFY_REG(hadc->Instance->CR, ADC_CR_BOOST, ADC_CR_BOOST_0);
 }
 else if (freq <= 25000000UL)
 {
 MODIFY_REG(hadc->Instance->CR, ADC_CR_BOOST, ADC_CR_BOOST_1);
 }
 else /* if(freq > 25000000UL) */
 {
 MODIFY_REG(hadc->Instance->CR, ADC_CR_BOOST, ADC_CR_BOOST_1 | ADC_CR_BOOST_0);
 }

The /2 prescaled frequency seems to have the same range as Rev Y. So, I think it's safe to simply double fADC to get the correct sample rate. CubeMX does not know this, and sets the wrong ADC clock prescale every time I use it :-(.

I think the /2 divider was not added to limit the ADC sample rate, they probably needed a clock signal with double the frequency inside the ADC circuit.