Skip to main content
antonius
Associate III
April 11, 2014
Question

Decoding bmp ?

  • April 11, 2014
  • 90 replies
  • 37500 views
Posted on April 11, 2014 at 11:21

Guys,

Does anyone of you have experience on decoding bmp ?

I want to display bmp file to my LCD...

Any clues ?

thanks

#i-have-a-clue
    This topic has been closed for replies.

    90 replies

    Andrew Neil
    Super User
    April 11, 2014
    Posted on April 11, 2014 at 21:39

    There is nothing in the BMP file format that's specific to STM32 - so just google it...

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Tesla DeLorean
    Guru
    April 11, 2014
    Posted on April 11, 2014 at 21:58

    There are several formats, you'll need to decode the header, figure out the dimensions, figure out the colour depth or palette tables, and then convert the format into one that is suitable for your display.

    As I recall some of the raster formats have the image paint from bottom-to-top, where as displays tend to be the other way round.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    antonius
    antoniusAuthor
    Associate III
    April 12, 2014
    Posted on April 12, 2014 at 03:12

    could you suggest me the keywords ?

    I read already the first 56 bytes is the information of the picture,

    so I just jump on it....

    In my mind now is

    320x240, so, the first line of the picture is 1x240, and repeat it until ...to complete the picture....

    I'll make a test with simple black and white 320x240, (box shape) to understand the idea, am I right ?

    Please see the file test_lcd.bmp....I'll use it for a test...or I need simpler to understand the idea ?

    thanks

    ________________

    Attachments :

    test_lcd.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Ds&d=%2Fa%2F0X0000000bkt%2Fv8EB0ALhGNn9677rz6MNSQYnLsx40lfaa3070mU2jM0&asPdf=false
    antonius
    antoniusAuthor
    Associate III
    April 12, 2014
    Posted on April 12, 2014 at 03:26

    I saw hexa editor, mostly FF on test_lcd.bmp ?0690X00000602sxQAA.jpg

    Tesla DeLorean
    Guru
    April 12, 2014
    Posted on April 12, 2014 at 14:13

    The picture data begins are 0x3E (62)

    You'd need to decode the bit stream, describing each line, into a pixel format suitable for your display. It's a monochrome image, black/white going by the RGB palette.

    http://www.ue.eti.pg.gda.pl/fpgalab/zadania.spartan3/zad_vga_struktura_pliku_bmp_en.html

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    antonius
    antoniusAuthor
    Associate III
    April 16, 2014
    Posted on April 17, 2014 at 01:26

    Is it possible like this ?

    
    LCD_WriteRAM_Prepare(); 
    /* Prepare to write GRAM */
    
    LCD_Clear(Yellow);
    
    res = f_open( &fsrc , 
    ''test.bmp''
    , FA_READ ); 
    
    //res = f_open( &fsrc , ''Demo.TXT'' , FA_READ); 
    
    printf
    (
    ''res value = ''
    );
    
    sprintf
    (temp_buffer,
    ''%.2d''
    ,res);
    printf
    (temp_buffer);
    printf
    (
    ''
    ''
    );
    
    printf
    (
    ''Content of the file :''
    );
    
    NEXT_LINE;
    
    while
    (f_gets(line, 
    sizeof
    line, &fsrc))
    
    printf
    (line);
    
    
    
    while
    (y <320)
    
    {
    
    x = 0;
    
    while
    (x <240)
    
    {
    
    
    //LCD_SetPoint (x, y, 0x0F0F);
    
    LCD_DrawPicture(0,0,239,319,line);
    
    delay_ms(1);
    
    
    x = x +1;
    
    }
    
    y = y +1;
    
    } 
    
    f_close(&fsrc);

    Tesla DeLorean
    Guru
    April 17, 2014
    Posted on April 17, 2014 at 02:34

    Is it possible like this?

    Not so much, I think you need to familiarize yourself with C File IO (and FatFs variants) and manipulating blocks of data.

    http://rakanalysis.wordpress.com/2012/04/27/566/

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    April 17, 2014
    Posted on April 17, 2014 at 04:34

    This is cruder than I'd like,

    // a more general solution would read dimensions from header
    // and handle errors, etc.
    // For the specific BMP, 1-bit per pixel, 320x240
    {
    int i, x, y;
    res = f_open(&fsrc, ''test.bmp'', FA_READ);
    f_seek(&fsrc, 0x3E, F_SEEK_SET); // Seek to the data
    for(y=0; y<320; y++)
    {
    for(x=0; x<240; x+=8) // advance 8 pixels (one byte of bits)
    {
    uint8_t b;
    UINT bytesread;
    f_read(&fsrc, &b, 1, &bytesread); // Read byte
    for(i=0; i<8; i++) // Process bits in byte, MSB first
    {
    if (b & 0x80) // Pixel On?
    LCD_SetPoint(x + i, y, 0x0F0F); // Colour
    else
    LCD_SetPoint(x + i, y, 0x0000); // Black
    b <<= 1;
    }
    } // x
    } // y
    f_close(&fsrc);
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    antonius
    antoniusAuthor
    Associate III
    April 17, 2014

    Posted on April 17, 2014 at 06:45

    I modify a little bit,

    f_seek(&fsrc, 0x3E, F_SEEK_SET); // Seek to the data <== I can't find SEEK_SET so I commented out, It can display bmp but smaller and 4 times, do I miss something in the loop ? suppose to be : 

     I got : 0690X00000602tHQAQ.jpg

     


    LCD_SetCursor(0,0);

    res = f_open(&fsrc, ''test1.bmp'', FA_READ);


    //f_seek(&fsrc, 0x3E, F_SEEK_SET); // Seek to the data

    //f_lseek(&fsrc, 0x0A);


    for(y=0; y<320; y++)

    {

    for(x=0; x<240; x+=2) // advance 8 pixels (one byte of bits)

    {

    uint8_t b;

    UINT bytesread;


    f_read(&fsrc, &b, 1, &bytesread); // Read byte


    for(i=0; i<8; i++) // Process bits in byte, MSB first

    {

    if (b & 0x80) // Pixel On?

    LCD_SetPoint(x+1, y, 0x0000); // Colour

    else

    LCD_SetPoint(x+i, y, 0xF0F0); // Black


    b <<= 1;

    }

    } // x

    } // y


    f_close(&fsrc);

     

    thanks

    antonius
    antoniusAuthor
    Associate III
    April 17, 2014
    Posted on April 17, 2014 at 06:51

    if I used

    1.
    for
    (y=0; y<320; y++)
    2.
    {
    3.
    for
    (x=0; x<240; x+=8) 
    // advance 8 pixels (one byte of bits)

    I got : 0690X00000602tMQAQ.jpg Do you have a clue ? thanks