Skip to main content
KBumS
Associate II
Aug 12, 2019 5:35 AM UTC
Solved

CAN communication between two NUCELO-F446RE ?

Hello! I'm using two STM32F446RE (NUCELO-64) boards through CAN communication, we want to perform CAN operation with one slave as master.

How do I know how to ensure that CUBEMX is communicating with each other?

 

#CAN​  #Example​ #STM32CubeMX​

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 15, 2026 5:07 PM UTC

Hello, 

Even this is an old topic, this is my answer (in case someone else is landing at this post:)

1- There is no master/slave concept in CAN protocol. Any CAN node on the bus is a transmitter or receiver without any permission of another CAN node on the bus.

2- Check out these knowledge base articles: 

Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 1)

Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 2)

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 15, 2026 5:07 PM UTC

Hello, 

Even this is an old topic, this is my answer (in case someone else is landing at this post:)

1- There is no master/slave concept in CAN protocol. Any CAN node on the bus is a transmitter or receiver without any permission of another CAN node on the bus.

2- Check out these knowledge base articles: 

Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 1)

Using CAN (bxCAN) in Normal mode with STM32 microcontrollers (Part 2)

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.