B-L462E-CELL1 eSIM activation is not allowed in this PLMN
- 5 replies
- 2805 views
Hello,
After purchasing the pre-configured Truphone eSIM B-L462E-CELL1 kit and following the eSIM activation steps, I still haven't seen the eSIM marked as activated on the Truphone IoT dashboard after one day.
I've also seen others inquire about this issue and have followed the advice to set 'at%nwoper' to "TRUPHONE" in the response, but the eSIM still cannot be activated.
(reference: https://community.st.com/t5/stm32-mcus-embedded-software/b-l462e-cell1-esim-activation-failed/m-p/617775)
Log:
AUTOM TASK: WAITING_FOR_NETWORK_STATUS_STATE - POLLING_TIMER_EVENT
*********** CST_network_status_test_mngt ********
ATParser:*** SEND (size=10) ***
AT+CEREG?<CR>
<CR><LF>
+CEREG: 2,3<CR><LF>
ATCModem:NetworkState (EPS) = REGISTRATION_DENIED
<CR><LF>
OK<CR><LF>
ATParser:*** SEND (size=9) ***
AT+CREG?<CR>
<CR><LF>
+CREG: 2,0<CR><LF>
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
<CR><LF>
OK<CR><LF>
ATParser:*** SEND (size=9) ***
AT%CEER?<CR>
<CR><LF>
%CEER: 1,"NAS-EMM","ATTACH","REJECT",#14,EPS_SERVICES_NOT_ALLOWED_IN_THIS_PLMN<CR><LF>
<CR><LF>
OK<CR><LF>
ATParser:*** SEND (size=9) ***
AT+COPS?<CR>
<CR><LF>
+COPS: 0<CR><LF>
<CR><LF>
OK<CR><LF>
ATParser:*** SEND (size=7) ***
AT+CSQ<CR>
<CR><LF>
+CSQ: 99,99<CR><LF>
<CR><LF>
OK<CR><LF>
-Sig quality rssi : 99
-Sig quality ber : 99
<CR><LF>
%NOTIFYEV:"SIMREFRESH",2,6,"00000000000000"<CR><LF>
Could you help to resolve this problem?
The attached file is full of logs.
Thanks a lot
Nelson