Skip to main content
Visitor II
Feb 16, 2026 2:00 PM UTC
Question

RMCS-2303 Motor Driver Integration - speed control issue

I am successfully receiving feedback from the motor side, including the encoder values, which are being read accurately.
I am writing to update you on the motor control project and to seek your guidance on an issue I'm currently facing.
Project Configuration:
  • Microcontroller: STM32H723ZG
  • Motor Drivers: Rhino RMCS-2303 (Quantity: 2)
  • Motors: Rhino DC Motors (Quantity: 2)
Hardware Setup:
Motor 1 (Left Motor):
  • UART Communication: USART2 (PA2-TX, PA3-RX)
  • Control Pins: ENA (PC0), DIR (PC2), BRK (PC4)
  • Feedback: ADC (PA0) - Optional
  • Slave ID: 7
Motor 2 (Right Motor):
  • UART Communication: USART1 (PA9-TX, PA10-RX)
  • Control Pins: ENA (PC1), DIR (PC3), BRK (PC5)
  • Feedback: ADC (PA1) - Optional
  • Slave ID: 6
Current Status:
I have successfully implemented the basic motor control system with the following functionalities:
  • :white_heavy_check_mark: Forward movement (F command)
  • :white_heavy_check_mark: Backward movement (B command)
  • :white_heavy_check_mark: Left turn (L command)
  • :white_heavy_check_mark: Right turn (R command)
  • :white_heavy_check_mark: Encoder feedback reading from both motors
Issue Faced:
However, I am facing difficulty in controlling the motor speed dynamically. The motors continue to run at the same speed regardless of the speed command I send. I am unable to increase or decrease the speed using commands.
Could you please guide me on:
  1. The correct command format/protocol for speed control with RMCS-2303?
  2. Any specific register settings or UART command structure I should follow?
  3. Whether any additional configuration is required in the driver settings?
 

Screenshot 2026-02-16 184011.pngScreenshot 2026-02-16 192543.pngScreenshot 2026-02-16 192614.png

1 reply

GMA
ST Technical Moderator
Mar 11, 2026 9:12 AM UTC

Hello @Ritika_10,

As mentioned here, "The goal of this e-Community is to provide a peer-to-peer and direct support for people using ST products". 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA