Skip to main content
Associate II
Aug 21, 2024 8:56 AM UTC
Question

Motor profiler 1.2.9 unable to spin motor

Hi, 

I am using motor workbench 6.3 along with stm32cube mx 6.12 and stm32cubeIDE 1.16.0. The hardware is a F303RE nucleo board with IHM08M1 motor board. The motor is a generci A2212 1000kV drone motor with a maximum current of 10A. 

C3, C5, C7 are removed as per https://www.st.com/resource/en/data_brief/x-nucleo-ihm08m1.pdf
Jumper JP1 & JP2 are on FOC. J5 & J6 are on 3 shunt measurement.

The motor profiler runs up to 28%, does not spin the motor and goes into "Motor profiler is taking too long error" 

I have configured the DSP libraries in the project properties and also added "pMCIList[M1] = &Mci[M1];" to solve the hardfault handler error. 

 

While generating the code I get "Attr not supported : Dmpu" error but I have been advised that it is not a serious error. https://community.st.com/t5/stm32-mcus-motor-control/mc-6-3-with-mx6-12-attr-not-supported-dmpu/m-p/704970#M10610

Neither motor profiler nor motor pilot work at the moment. Please advise. 

IMG_20240821_142029810.jpg

code generation.png

 

 

the measurement is taking too time.png

motor profiler setting.png

This topic has been closed for replies.

3 replies

GMA
ST Technical Moderator
Sep 2, 2024 8:56 AM UTC

Hello @Sujoy_B,

Thank you for your report. We are investigating this issue, and we will come back to you shortly once we know more about it.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
GMA
ST Technical Moderator
Sep 3, 2024 2:58 PM UTC

Hello @Sujoy_B,

We are still investigating the issue, but if your purpose is profiling the motor, disabling the "MCU Load measurement" feature should be functional.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
ST Employee
May 20, 2025 9:42 AM UTC

Hello @Sujoy_B ,

 

This issue has been fixed with the solution proposed above in our new MCSDK 6.4.0 release,
so feel free to download it and try if it solved correctly your issue reported in this post.

Kind Regards.

If you agree with my answer, please accept it by clicking on 'Accept as solution'.