Skip to main content
Associate II
June 16, 2025
Question

Does the STEVAL-CTM010V1 support 115200 baudrate ?

Hello,

      I use MCWB 6.4.0 & Motor Pilot 6.4.0, STLINK V3 MINIE.

      Motor Pilot can not discover STEVAL-CTM010V1 board.

      And  I find that MCU can receive datas at buadrate 1200 to 14400, but failed at 19200  or  more fast .

      Does the STEVAL-CTM010V1 support 115200 baudrate ?  Or PC817B doesn't  support this baudrate?

 

      this issue seems like this one, https://community.st.com/t5/stm32-mcus-motor-control/steval-ctm010v1-board-can-not-work/m-p/241708#M4301 

This topic has been closed for replies.

2 replies

wcx8229Author
Associate II
June 17, 2025

so is steval-ctm010v1 board , even if  exist some years,  a mature solution ?

GMA
ST Technical Moderator
July 7, 2025

Hello @wcx8229,

According to this post, you are able to connect the MC Pilot with your board. Could you share what was the issue root cause?

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA