Skip to main content
Visitor II
April 16, 2024
Question

BLDC motor control using Temperature sensor

Hi all, I have been trying to control my BLDC motor with an condition where if the surrounding temperature increases a threshold temperature the bldc motor should turn fast else slow. I am using lm35 as temperature sensor, i was able to interface this using stm32 nucleo g431rb board , esc and lm35 but i want to interface this through the code generated from motor control workbench. I need few insights on this, the code is generated for P-Nucleo-IHM03 motor control pack with FOC control algorithm.

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
June 20, 2024

Hello @hemanthgowdas,

As mentioned in MCSDK 6.3.0 post, a ST Motor Control Board Designer (STMCBD) tool is provided and gives to the users the ability to describe their own motor control hardware through an easy-to-use graphical interface. This description can then be used in the ST Motor Control Workbench.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA