Skip to main content
Associate III
Dec 10, 2025 5:04 AM UTC
Solved

Zephyr RTOS on Nucleo-F411RE ?

Hi 

Is it possible to run Zephyr RTOS on the STM32F411RET6 Nucleo board? If it is possible, how can I set up and use Zephyr RTOS on it? Please suggest the steps.

T_Hamdi
T_HamdiBest answer
ST Employee
Dec 10, 2025 10:46 AM UTC

hello @Kumar123 

Yes, it is possible to run Zephyr RTOS on the STM32F411RET6 Nucleo board. For detailed information on board specifications, supported features, and configuration, you can refer to the official Zephyr documentation here:
Zephyr Board: Nucleo F411RE.

also to get started with Zephyr RTOS on the STM32F411RET6 nucleo board, you can follow the official Getting Started Guide provided by the Zephyr Project:
Getting Started Guide — Zephyr Project Documentation.

 

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Hamdi Teyeb"

3 replies

T_Hamdi
T_HamdiBest answer
ST Employee
Dec 10, 2025 10:46 AM UTC

hello @Kumar123 

Yes, it is possible to run Zephyr RTOS on the STM32F411RET6 Nucleo board. For detailed information on board specifications, supported features, and configuration, you can refer to the official Zephyr documentation here:
Zephyr Board: Nucleo F411RE.

also to get started with Zephyr RTOS on the STM32F411RET6 nucleo board, you can follow the official Getting Started Guide provided by the Zephyr Project:
Getting Started Guide — Zephyr Project Documentation.

 

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Hamdi Teyeb"
Andrew Neil
Super User
Dec 29, 2025 11:06 AM UTC

Follow-on question: Zephyr Blinky LED example not blinking.

 

@Kumar123 - please keep to one question per thread.


Edited to correct link.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Kumar123Author
Associate III
Dec 29, 2025 11:21 AM UTC

Hi Andrew Neil

The above link are not open.