Skip to main content
Associate III
Dec 27, 2025 11:31 AM UTC
Question

Zephyr Blinky LED example not blinking

Split from Zephyr RTOS on Nucleo-F411RE ? - which has been answered.

This is a new question.


Hi T_Hamdi

Thank you for your response.

I have installed the Zephyr IDE and used the Blinky LED example. The firmware was flashed successfully; however, the LED is not glowing.

I have attached an image for your reference. Please take a look.

1 reply

T_Hamdi
ST Employee
Dec 29, 2025 10:24 AM UTC

Hello @Kumar123,

I see in the image that the .hex file is flashed using the J-Link debugger. Do you have a J-Link connected to the board, or are you using the ST-Link included on the board?

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Hamdi Teyeb"