Skip to main content
Associate II
Jul 8, 2025 1:44 PM UTC
Question

XSPI / XSPIM / EXTMem in Application code for FileX / LevelX

I have a basic FSBL Load and Run application on the NUCLEO-N657 that loads an application from flash into the internal SRAM of the MCU.

 

Since the N6 has no internal flash, I would like to allocate a portion of the external flash memory to a Fat/FileX volume that the loaded application can use.

What's the preferred method of creating a custom LevelX nor driver in Application for using the OSPI Flash?  Should I use the EXTMem manager to abstract the read/writes, or should I integrate the XSPI2 driver directly into the custom LevelX nor controller?

 

Current Attempt, using EXTMem_manager within custom nor controller:

In my FSBL, I successfully init XSPI2, XSPIM, and the EXTMEM_Manager to load and run the application from flash. (Tutorial) 

 

However, once the application begins initialization, the app cannot re-init XSPI2 and times out with a busy error.  If I bypass the init of XSPI2, then the EXTMEM manager times out trying to access the XSPI2 peripheral.

// appli main.c

int main(void)
{
 HAL_Init();

 MX_GPIO_Init();
 MX_ETH1_Init();
 MX_USB1_OTG_HS_USB_Init();
 MX_HASH_Init();
 MX_RNG_Init();
 MX_XSPI2_Init(); // <- Unmodified, throws an error on HAL_XSPI_Init()
 SystemIsolation_Config();
 MX_EXTMEM_MANAGER_Init();

 MX_ThreadX_Init();
}

Seems like trying to re-init the peripheral is causing errors, since the peripheral was initialized and used to load the application.  If I return early in XSPI2_Init(), then the app runs, but the XSPI2 bus has a timeout after the standard 5000 ms.

// lx_stm32_nor_custom_driver.c
#include "lx_stm32_nor_custom_driver.h"

/* USER CODE BEGIN Includes */
#include "stm32_extmem_conf.h"
#include "extmem_manager.h"
#include "stm32_extmem.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
typedef enum
{
 FLASH_OK,
 FLASH_ERROR_UNSUPPORTED_MEMORY, /* !< unsupported memory type */
 FLASH_ERROR_NOBASEADDRESS, /* !< not base address for the memory */
 FLASH_ERROR_MAPPEDMODEFAIL, /* !< */
 FLASH_ERROR_COPY,
} FLASHStatus_TypeDef;
/* USER CODE END PTD */

/* USER CODE BEGIN PV */
static uint8_t block_erase_verify_buf[LX_STM32_NOR_FLASH_BLOCK_SIZE] = {0};
/* USER CODE END PV */

static UINT lx_nor_driver_read(ULONG *flash_address, ULONG *destination, ULONG words);
static UINT lx_nor_driver_write(ULONG *flash_address, ULONG *source, ULONG words);
static UINT lx_nor_driver_block_erase(ULONG block, ULONG erase_count);
static UINT lx_nor_driver_block_erased_verify(ULONG block);

#ifndef LX_DIRECT_READ

#ifndef NOR_SECTOR_BUFFER_SIZE
#define NOR_SECTOR_BUFFER_SIZE 512
#endif

static ULONG nor_sector_memory[NOR_SECTOR_BUFFER_SIZE];
#endif

UINT lx_stm32_nor_custom_driver_initialize(LX_NOR_FLASH *nor_flash)
{
 UINT ret = LX_SUCCESS;

 ULONG total_blocks = 0;
 ULONG words_per_block = 0;

 /* USER CODE BEGIN Init_Section_0 */

 /* USER CODE END Init_Section_0 */

 nor_flash->lx_nor_flash_total_blocks = total_blocks;
 nor_flash->lx_nor_flash_words_per_block = words_per_block;

 /* USER CODE BEGIN Init_Section_1 */

 /* USER CODE END Init_Section_1 */

 nor_flash->lx_nor_flash_driver_read = lx_nor_driver_read;
 nor_flash->lx_nor_flash_driver_write = lx_nor_driver_write;

 nor_flash->lx_nor_flash_driver_block_erase = lx_nor_driver_block_erase;
 nor_flash->lx_nor_flash_driver_block_erased_verify = lx_nor_driver_block_erased_verify;

#ifndef LX_DIRECT_READ
 nor_flash->lx_nor_flash_sector_buffer = nor_sector_memory;
#endif

 /* USER CODE BEGIN Init_Section_2 */

 /* USER CODE END Init_Section_2 */

 return ret;
}

/* USER CODE BEGIN USER_CODE_SECTION_2 */

/* USER CODE END USER_CODE_SECTION_2 */

static UINT lx_nor_driver_read(ULONG *flash_address, ULONG *destination, ULONG words)
{
 UINT ret = LX_SUCCESS;
 const uint32_t MapAddress = (uint32_t)(flash_address + LX_STM32_NOR_FLASH_FS_START_ADDRESS_OFFSET);

 /* USER CODE BEGIN NOR_READ */
 if (EXTMEM_OK != EXTMEM_Read(EXTMEMORY_1,
 MapAddress,
 (uint8_t *)destination,
 words * sizeof(ULONG)))
 {
 printf("lx_nor_driver_read: EXTMEM_Read failed!\r\n");
 ret = LX_ERROR;
 }
 printf("lx_nor_driver_read: Read %lu words from address 0x%08lX\r\n", words, (unsigned long)flash_address + LX_STM32_NOR_FLASH_FS_START_ADDRESS_OFFSET);
 /* USER CODE END NOR_READ */

 return ret;
}

static UINT lx_nor_driver_write(ULONG *flash_address, ULONG *source, ULONG words)
{
 UINT ret = LX_SUCCESS;

 /* USER CODE BEGIN NOR_DRIVER_WRITE */
 if (EXTMEM_OK != EXTMEM_Write(EXTMEMORY_1,
 (uint32_t)(flash_address + LX_STM32_NOR_FLASH_FS_START_ADDRESS_OFFSET),
 (const uint8_t *)source,
 words * sizeof(ULONG)))
 {
 printf("lx_nor_driver_write: EXTMEM_WriteInMappedMode failed!\r\n");
 ret = LX_ERROR;
 }
 printf("lx_nor_driver_write: Written %lu words to address 0x%08lX\r\n", words, (unsigned long)flash_address + LX_STM32_NOR_FLASH_FS_START_ADDRESS_OFFSET);
 /* USER CODE END NOR_DRIVER_WRITE */

 return ret;
}

static UINT lx_nor_driver_block_erase(ULONG block, ULONG erase_count)
{

 UINT ret = LX_SUCCESS;

 /* USER CODE BEGIN NOR_DRIVER_BLOCK */
 if (EXTMEM_OK != EXTMEM_EraseSector(EXTMEMORY_1,
 ((uint32_t)(block * LX_STM32_NOR_FLASH_BLOCK_SIZE) + LX_STM32_NOR_FLASH_FS_START_ADDRESS_OFFSET),
 LX_STM32_NOR_FLASH_BLOCK_SIZE))
 {
 printf("lx_nor_driver_block_erase: EXTMEM_EraseSector failed!\r\n");
 ret = LX_ERROR;
 }
 printf("lx_nor_driver_block_erase: Erased block %lu, erase_count %lu\r\n", block, erase_count);
 /* USER CODE END NOR_DRIVER_BLOCK */

 return ret;
}

static UINT lx_nor_driver_block_erased_verify(ULONG block)
{
 UINT ret = LX_SUCCESS;

 /* USER CODE BEGIN NOR_DRIVER_VERIFY */
 EXTMEM_Read(EXTMEMORY_1,
 (uint32_t)((block * LX_STM32_NOR_FLASH_BLOCK_SIZE) + LX_STM32_NOR_FLASH_FS_START_ADDRESS_OFFSET),
 (uint8_t *)block_erase_verify_buf,
 LX_STM32_NOR_FLASH_BLOCK_SIZE);

 for (int i = 0; i < LX_STM32_NOR_FLASH_BLOCK_SIZE; i++)
 {
 if (block_erase_verify_buf[i] != 0xFF)
 {
 printf("lx_nor_driver_block_erased_verify: Block %lu not erased at word %d!\r\n", block, i);
 ret = LX_ERROR;
 break;
 }
 }
 /* USER CODE END NOR_DRIVER_VERIFY */

 return ret;
}

For reference, here's the FileX implementation to load the custom LevelX NOR driver:

// app_filex.c
#include "app_filex.h"
/* Main thread stack size */
#define FX_APP_THREAD_STACK_SIZE 1024 * 2
/* Main thread priority */
#define FX_APP_THREAD_PRIO 10

/* Main thread global data structures. */
TX_THREAD fx_app_thread;

/* USER CODE BEGIN PV */
FX_MEDIA nor_flash_disk;
/* FileX file instance */
FX_FILE fx_file;
uint32_t media_memory[LX_STM32_NOR_FLASH_BLOCK_SIZE / sizeof(uint32_t)];
/* USER CODE END PV */

void fx_app_thread_entry(ULONG thread_input);

UINT MX_FileX_Init(VOID *memory_ptr)
{
 UINT ret = FX_SUCCESS;
 TX_BYTE_POOL *byte_pool = (TX_BYTE_POOL *)memory_ptr;
 VOID *pointer;

 /*Allocate memory for the main thread's stack*/
 ret = tx_byte_allocate(byte_pool, &pointer, FX_APP_THREAD_STACK_SIZE, TX_NO_WAIT);

 /* Check FX_APP_THREAD_STACK_SIZE allocation*/
 if (ret != FX_SUCCESS)
 {
 return TX_POOL_ERROR;
 }

 /* Create the main thread. */
 ret = tx_thread_create(&fx_app_thread, FX_APP_THREAD_NAME, fx_app_thread_entry, 0, pointer, FX_APP_THREAD_STACK_SIZE,
 FX_APP_THREAD_PRIO, FX_APP_PREEMPTION_THRESHOLD, FX_APP_THREAD_TIME_SLICE, FX_APP_THREAD_AUTO_START);

 /* Check main thread creation */
 if (ret != FX_SUCCESS)
 {
 return TX_THREAD_ERROR;
 }

 /* Initialize FileX. */
 fx_system_initialize();

 return ret;
}

void fx_app_thread_entry(ULONG thread_input)
{
 UNUSED(thread_input);

 /* Format the NOR flash as FAT */
 UINT status = fx_media_format(&nor_flash_disk,
 fx_stm32_levelx_nor_driver, // Driver entry
 (VOID *)NOR_CUSTOM_DRIVER_ID, // Device info pointer
 media_memory, // Media buffer pointer
 sizeof(media_memory), // Media buffer size
 "NOR_FLASH_DISK", // Volume Name
 1, // Number of FATs
 32, // Directory Entries
 0, // Hidden sectors
 LX_STM32_NOR_FLASH_FS_PARTITION_SIZE /
 LX_STM32_NOR_FLASH_BLOCK_SIZE, // Total sectors
 LX_STM32_NOR_FLASH_BLOCK_SIZE, // Sector size
 8, // Sectors per cluster
 1, // Heads
 1); // Sectors per track

 /* Check if the format status */
 if (status != FX_SUCCESS)
 {
 Error_Handler();
 }

 /* Open the octo-SPI NOR Flash disk driver. */
 status = fx_media_open(&nor_flash_disk, "FX_LX_NOR_DISK", fx_stm32_levelx_nor_driver, (VOID *)NOR_CUSTOM_DRIVER_ID, media_memory, sizeof(media_memory));

 /* Check the media open status. */
 if (status != FX_SUCCESS)
 {
 Error_Handler();
 }
}

 

No matter what I try, XSPI2 times out on either infit or in EXTMem_Read in the application.

Screenshot 2025-07-08 081434.pngScreenshot 2025-07-08 081421.pngScreenshot 2025-07-08 081330.pngScreenshot 2025-07-08 081241.pngScreenshot 2025-07-08 081038.png

This topic has been closed for replies.

2 replies

Associate II
Jul 8, 2025 7:42 PM UTC

Changing the MX_XSPI2_Init() in the Application to not re-init XSPI2 allows the XSPIM and EXTMEM manager to initialize properly.  However, the EXTMEM_Read and Write functions seems to timeout, resulting in 

fx_media_format() returning FX_IO_ERROR.
//xspi.c

void MX_XSPI2_Init(void)
{

 /* USER CODE BEGIN XSPI2_Init 0 */

 /* USER CODE END XSPI2_Init 0 */

 XSPIM_CfgTypeDef sXspiManagerCfg = {0};

 /* USER CODE BEGIN XSPI2_Init 1 */
 hxspi2.Instance = XSPI2;
 hxspi2.Init.FifoThresholdByte = 4;
 hxspi2.Init.MemoryMode = HAL_XSPI_SINGLE_MEM;
 hxspi2.Init.MemoryType = HAL_XSPI_MEMTYPE_MACRONIX;
 hxspi2.Init.MemorySize = HAL_XSPI_SIZE_512MB;
 hxspi2.Init.ChipSelectHighTimeCycle = 1;
 hxspi2.Init.FreeRunningClock = HAL_XSPI_FREERUNCLK_DISABLE;
 hxspi2.Init.ClockMode = HAL_XSPI_CLOCK_MODE_0;
 hxspi2.Init.WrapSize = HAL_XSPI_WRAP_NOT_SUPPORTED;
 hxspi2.Init.ClockPrescaler = 0;
 hxspi2.Init.SampleShifting = HAL_XSPI_SAMPLE_SHIFT_NONE;
 hxspi2.Init.DelayHoldQuarterCycle = HAL_XSPI_DHQC_ENABLE;
 hxspi2.Init.ChipSelectBoundary = HAL_XSPI_BONDARYOF_NONE;
 hxspi2.Init.MaxTran = 0;
 hxspi2.Init.Refresh = 0;
 hxspi2.Init.MemorySelect = HAL_XSPI_CSSEL_NCS1;

 // // HAL_XSPI_DeInit(&hxspi2);
 // if (HAL_XSPI_Init(&hxspi2) != HAL_OK)
 // {
 // Error_Handler();
 // }

 sXspiManagerCfg.nCSOverride = HAL_XSPI_CSSEL_OVR_NCS1;
 sXspiManagerCfg.IOPort = HAL_XSPIM_IOPORT_2;
 sXspiManagerCfg.Req2AckTime = 1;
 if (HAL_XSPIM_Config(&hxspi2, &sXspiManagerCfg, HAL_XSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }

 return; // Skip generated code

 /* USER CODE END XSPI2_Init 1 */
 hxspi2.Instance = XSPI2;
 hxspi2.Init.FifoThresholdByte = 4;
 hxspi2.Init.MemoryMode = HAL_XSPI_SINGLE_MEM;
 hxspi2.Init.MemoryType = HAL_XSPI_MEMTYPE_MACRONIX;
 hxspi2.Init.MemorySize = HAL_XSPI_SIZE_512MB;
 hxspi2.Init.ChipSelectHighTimeCycle = 1;
 hxspi2.Init.FreeRunningClock = HAL_XSPI_FREERUNCLK_DISABLE;
 hxspi2.Init.ClockMode = HAL_XSPI_CLOCK_MODE_0;
 hxspi2.Init.WrapSize = HAL_XSPI_WRAP_NOT_SUPPORTED;
 hxspi2.Init.ClockPrescaler = 0;
 hxspi2.Init.SampleShifting = HAL_XSPI_SAMPLE_SHIFT_NONE;
 hxspi2.Init.DelayHoldQuarterCycle = HAL_XSPI_DHQC_ENABLE;
 hxspi2.Init.ChipSelectBoundary = HAL_XSPI_BONDARYOF_NONE;
 hxspi2.Init.MaxTran = 0;
 hxspi2.Init.Refresh = 0;
 hxspi2.Init.MemorySelect = HAL_XSPI_CSSEL_NCS1;
 if (HAL_XSPI_Init(&hxspi2) != HAL_OK)
 {
 Error_Handler();
 }
 sXspiManagerCfg.nCSOverride = HAL_XSPI_CSSEL_OVR_NCS1;
 sXspiManagerCfg.IOPort = HAL_XSPIM_IOPORT_2;
 sXspiManagerCfg.Req2AckTime = 1;
 if (HAL_XSPIM_Config(&hxspi2, &sXspiManagerCfg, HAL_XSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN XSPI2_Init 2 */

 /* USER CODE END XSPI2_Init 2 */
}

 

Attempting to DeInit and ReInit XSPI2 in the application causes the EXTMEM_Init to time out on initialization, even though the DeInit/ Init of XSPI2 and XSPIM do not throw any errors.

// xspi.c
void MX_XSPI2_Init(void)
{

 /* USER CODE BEGIN XSPI2_Init 0 */

 /* USER CODE END XSPI2_Init 0 */

 XSPIM_CfgTypeDef sXspiManagerCfg = {0};

 /* USER CODE BEGIN XSPI2_Init 1 */
 hxspi2.Instance = XSPI2;
 hxspi2.Init.FifoThresholdByte = 4;
 hxspi2.Init.MemoryMode = HAL_XSPI_SINGLE_MEM;
 hxspi2.Init.MemoryType = HAL_XSPI_MEMTYPE_MACRONIX;
 hxspi2.Init.MemorySize = HAL_XSPI_SIZE_512MB;
 hxspi2.Init.ChipSelectHighTimeCycle = 1;
 hxspi2.Init.FreeRunningClock = HAL_XSPI_FREERUNCLK_DISABLE;
 hxspi2.Init.ClockMode = HAL_XSPI_CLOCK_MODE_0;
 hxspi2.Init.WrapSize = HAL_XSPI_WRAP_NOT_SUPPORTED;
 hxspi2.Init.ClockPrescaler = 0;
 hxspi2.Init.SampleShifting = HAL_XSPI_SAMPLE_SHIFT_NONE;
 hxspi2.Init.DelayHoldQuarterCycle = HAL_XSPI_DHQC_ENABLE;
 hxspi2.Init.ChipSelectBoundary = HAL_XSPI_BONDARYOF_NONE;
 hxspi2.Init.MaxTran = 0;
 hxspi2.Init.Refresh = 0;
 hxspi2.Init.MemorySelect = HAL_XSPI_CSSEL_NCS1;

 HAL_XSPI_DeInit(&hxspi2);
 if (HAL_XSPI_Init(&hxspi2) != HAL_OK)
 {
 Error_Handler();
 }

 sXspiManagerCfg.nCSOverride = HAL_XSPI_CSSEL_OVR_NCS1;
 sXspiManagerCfg.IOPort = HAL_XSPIM_IOPORT_2;
 sXspiManagerCfg.Req2AckTime = 1;
 if (HAL_XSPIM_Config(&hxspi2, &sXspiManagerCfg, HAL_XSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }

 return; // Skip generated code
/* USER CODE END XSPI2_Init 1 */
 hxspi2.Instance = XSPI2;
 hxspi2.Init.FifoThresholdByte = 4;
 hxspi2.Init.MemoryMode = HAL_XSPI_SINGLE_MEM;
 hxspi2.Init.MemoryType = HAL_XSPI_MEMTYPE_MACRONIX;
 hxspi2.Init.MemorySize = HAL_XSPI_SIZE_512MB;
 hxspi2.Init.ChipSelectHighTimeCycle = 1;
 hxspi2.Init.FreeRunningClock = HAL_XSPI_FREERUNCLK_DISABLE;
 hxspi2.Init.ClockMode = HAL_XSPI_CLOCK_MODE_0;
 hxspi2.Init.WrapSize = HAL_XSPI_WRAP_NOT_SUPPORTED;
 hxspi2.Init.ClockPrescaler = 0;
 hxspi2.Init.SampleShifting = HAL_XSPI_SAMPLE_SHIFT_NONE;
 hxspi2.Init.DelayHoldQuarterCycle = HAL_XSPI_DHQC_ENABLE;
 hxspi2.Init.ChipSelectBoundary = HAL_XSPI_BONDARYOF_NONE;
 hxspi2.Init.MaxTran = 0;
 hxspi2.Init.Refresh = 0;
 hxspi2.Init.MemorySelect = HAL_XSPI_CSSEL_NCS1;
 if (HAL_XSPI_Init(&hxspi2) != HAL_OK)
 {
 Error_Handler();
 }
 sXspiManagerCfg.nCSOverride = HAL_XSPI_CSSEL_OVR_NCS1;
 sXspiManagerCfg.IOPort = HAL_XSPIM_IOPORT_2;
 sXspiManagerCfg.Req2AckTime = 1;
 if (HAL_XSPIM_Config(&hxspi2, &sXspiManagerCfg, HAL_XSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN XSPI2_Init 2 */

 /* USER CODE END XSPI2_Init 2 */
}

 Here's a screen shot of the call stack for where EXTMEM_Init() is hanging, and eventually entering hard fault due to timeout with the above version of XSPI2_Init():

Screenshot 2025-07-08 144035.png

ST Technical Moderator
Jul 10, 2025 8:30 AM UTC

Hello @musicmindmachine 

It is better to directly use the XSPI2 driver in your custom LevelX NOR controller. You can get inspired from the example below: 

STM32CubeN6/Projects/STM32N6570-DK/Applications/FileX/Fx_uSD_File_Edit at main · STMicroelectronics/STM32CubeN6 · GitHub

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om