Skip to main content

4 replies

ST Technical Moderator
Feb 6, 2026 1:14 PM UTC

Hi @xGloooM 

I will provide a guideline as FAQ to enter EPR mode as sink.

However, as EPR voltages are not supported on our hardware, VBUS value management will be kept on 5V value for this demonstration purpose package (whatever the contract negotiated between SRC and SNK sides). This limitation does not prevent from exercising the complete USBPD EPR stack for reaching either SPR or EPR contract negotiation. This limitation could be disabled (in case management of higher voltages is managed on application side and supported by hardware), but you have to manage your power management at your own risk.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
xGloooMAuthor
Associate II
Feb 7, 2026 11:57 AM UTC

I've also found strange behaviour in the stack.

After receiving PDOs in EPR mode, it calls USBPD_DPM_SetDataInfo with USBPD_CORE_DATATYPE_RCV_SRC_PDO with the Size of SPR + EPR PDOs, but empty last PDOs, which corresponds to EPR ones.

Is it a bug?

xGloooM_1-1770465563418.png

 

 

ST Technical Moderator
Feb 10, 2026 2:58 PM UTC

Hi @xGloooM 

I assume you this is an implementation issue. You may need to differentiate between DPM_ListOfRcvSRCEPRPDO and DPM_ListOfRcvSRCPDO. You need to store SPR and EPR PDOs in two separate arrays.

case USBPD_CORE_DATATYPE_RCV_SRC_PDO_EPR :
 if (*Size <= (USBPD_MAX_NB_PDO * 4U))
 {
 uint8_t* pdo;
 DPM_Ports[PortNum].DPM_NumberOfRcvSRCEPRPDO = (*Size / 4U);
 /* Copy EPR PDO data in DPM Handle field */
 for (uint32_t index = 0; index < (*Size / 4U); index++)
 {
 pdo = (uint8_t*)&DPM_Ports[PortNum].DPM_ListOfRcvSRCEPRPDO[index];
 (void)memcpy(pdo, (Ptr + (index * 4U)), (4U * sizeof(uint8_t)));
 }
 }
 break;

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
xGloooMAuthor
Associate II
Feb 11, 2026 9:06 AM UTC

Yes, case USBPD_CORE_DATATYPE_RCV_SRC_PDO_EPR is handled separately. But the problem is inside USBPD_CORE_DATATYPE_RCV_SRC_PDO (non-EPR), where 

DPM_Ports[PortNum].DPM_NumberOfRcvSRCPDO = (*Size / 4U);

 can't work properly after entering EPR_Mode, as the stack returns Size = 28, 28/4=7; however, SPR has only 6 PDOs and 1 EPR PDO.

I've workaround it as

 uint32_t pdos_cnt = 0;

 for (uint32_t index = 0; index < (Size / 4); index++)
 {
 rdo = (uint8_t*)&DPM_Ports[PortNum].DPM_ListOfRcvSRCPDO[index];
 (void)memcpy(rdo, (Ptr + (index * 4u)), (4u * sizeof(uint8_t)));
 if (*rdo != 0) {
 pdos_cnt++;
 }
 }
 DPM_Ports[PortNum].DPM_NumberOfRcvSRCPDO = pdos_cnt;