Skip to main content
brokenkeyboard
Associate II
February 21, 2021
Question

USB Battery Charging (BC)

Hello,

When using an MCU with USB FS capabilities, do I need an external IC to be able if an SDP, a DCP or a CDP was plugged in ? Or can the MCU do the job ? Apparently yes, but I struggle to find evidence of this, especially in the datasheets or in the HAL drivers descriptions.

Also I heard that the 0.5A max current of USB 2.0 was a minimal maximum, i.e a USB compliant port with nothing else plugged has to be able at least 0.5A through negotiation during the enumeration, but eventually could give more. But I think I got that wrong since it looks like the USB 2.0 protocol itself doesn't allow to ask for more than 0.5A...

This topic has been closed for replies.