cancel
Showing results for 
Search instead for 
Did you mean: 

Battery charging detector(USB_BCDR) of STM32F04 only works one time

jiangpen
Associate II
Posted on June 07, 2018 at 06:46

Hi All,

 I am working on a charger based on STM32F04.

It can detect the SDP or DCP when PC or charger connected, but it only works one time. That means when I unplug and plug the USB, it always detects as SDP.

I believe it might be the USB is not uninitialized correctly, but really don't know which parts cause this problem.

When I do a software reset, then the correct port type can be detected. So I am not sure what USB uninitialized should be done.

thanks

 if(vbus_detect)

        {

            if(usb_init)

            {

                USBD_Stop(&hUsbDeviceFS);

                USBD_DeInit(&hUsbDeviceFS);

                HAL_Delay(10);

                *(uint16_t *)(USB_BCDR) &= (uint16_t)(~(USB_BCDR_DPPU));

                   __IO uint16_t * cntr=(uint16_t *)(USB_CNTR);

                (*cntr)= USB_CNTR_FRES

            }

            USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);

            USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC);

            USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS);

            charge_port_detect();

            USBD_Start(&hUsbDeviceFS);

            usb_init=true;

}

void charge_port_detect()

{

    __IO uint16_t * bcdr=(uint16_t *)(USB_BCDR);

    (*bcdr) |= (USB_BCDR_BCDEN);

    HAL_Delay( 300 );

    (*bcdr) |= (USB_BCDR_PDEN);

    HAL_Delay( 300 );

    lastport=port;

    /* If Charger detect ? */

    if( (*bcdr) & USB_BCDR_PDET )

    {

        /* Start secondary detection to check connection to Charging Downstream

         Port or Dedicated Charging Port */

        (*bcdr) &= ~(USB_BCDR_PDEN);

        (*bcdr) |= (USB_BCDR_SDEN);

        HAL_Delay( 300 );

        /* If CDP ? */

        if( (*bcdr) & USB_BCDR_SDET )

        {

            /* Dedicated Downstream Port DCP */

            port = PORT_DCP;

        }

        else

        {

            /* Charging Downstream Port CDP */

            port = PORT_CDP;

        }

    }

    else /* NO */

    {

        /* Standard Downstream Port */

        port = PORT_SDP;

    }

    (*bcdr) &= ~(USB_BCDR_BCDEN);

}

#usb-stm32f04-battery-charging-detector(usb_bcdr)
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on June 07, 2018 at 11:58

It appears that you leave secondary detection enabled (SDEN bit set). Try to switch it off after the detection.

JW