Skip to main content
Associate
Dec 11, 2025 6:39 AM UTC
Question

U5 Nucleo + APS6404 + ThreadX: hard fault using memory-mapped QSPI for thread stack

I have set up a STM32U5 nucleo board with an additional 8M of memory using an APS6404, following the example in AN5050. Initial setup was straightforward, but trying to create a ThreadX thread that uses an array in that section of memory as its stack isn't working -- local variables within the thread are fine, but function calls like printf("foo") or tx_thread_sleep(10) cause a hard fault.

This is my first project using a STM32 microcontroller, and think I'm missing some fundamental understanding of how this is supposed to work -- any suggestions for what I've missed / what I should try?

------------------ Details about what I'm trying ----------------- 

After following the steps given in AN5050, I updated my .ld file to create a corresponding memory section:

MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 2496K
SRAM4 (xrw) : ORIGIN = 0x28000000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 4096K
OCTOSPI1 (xrw) : ORIGIN = 0x90000000, LENGTH = 8M
}

SECTIONS
{
.octospi1 :
{
. = ALIGN(4);
KEEP(*(.octospi1))
. = ALIGN(4);
} > OCTOSPI1

// [...snip...]

}

 

Then, I tried to assign a thread's stack to that section:
(This is following the example at https://community.st.com/t5/stm32-mcus/how-to-create-a-thread-using-azurertos-and-stm32cubeide/ta-p/49418, with __attribute__ added)

 
 
uint8_t memory_stack[8192] __attribute__((section(".octospi1")));
TX_THREAD memory_thread;

UINT App_ThreadX_Init(VOID *memory_ptr) {
// [...snip...]
ret = tx_thread_create(&memory_thread, "memory demo thread",
memory_thread_entry, 0,
memory_stack, 8192, 4, 1,
TX_NO_TIME_SLICE, TX_AUTO_START);
// [...snip...]
}

Inside memory_thread_entry, individual variables work fine (and I've used the Memory Browser to confirm that they are in the .octospi1 section), but calls to e.g. printf("foo") or tx_thread_sleep(10) cause a hard fault. If I leave out the __attribute__ call in the above code, all calls in the thread work as I expect.

2 replies

KDJEM.1
ST Technical Moderator
Jan 12, 2026 3:27 PM UTC

Hello @laura_l and welcome to the community;

 

First of all, I apologize for my late reply. I recommend you to look at How to debug a HardFault on an Arm® Cortex®-M STM32 - STMicroelectronics Community article may help you to find the HardFault root cause.

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
AE_APMemory
Graduate
Mar 27, 2026 3:29 PM UTC

Hi @laura_l ,

Could you share the reason for using such a large stack size?

If you need to define a large array in external memory (PSRAM) within a thread, you could declare it as follows:

void memory_thread_entry(void)
{
 static uint8_t big_buffer[8192] __attribute__((section(".octospi1")));
}

The thread stack could be allocated in RAM or SRAM4 and kept to a small size.

 

Panda