Skip to main content
MEde.1
Associate III
Mar 6, 2023 9:30 AM UTC
Question

Trying to compile Ultrasound FFT from SW_Source using QT and getting an error message that libhs_datalog.dll is corrupt.

The specific message is LNK1107: invalid or corrupt file cannot read at 0x3F8

This topic has been closed for replies.

17 replies

Visitor II
Nov 25, 2023 2:17 AM UTC

@SimonePradolini 

Hi SPRAD.1,
Any progress to resolve this issue? 

SimonePradolini
ST Technical Moderator
Nov 29, 2023 11:39 AM UTC

Hello,

I'm sorry, but the maintenance release planned for the last quarter has been moved to the end of the year.

 

Best regards

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
AScha.3
Super User
Nov 29, 2023 11:48 AM UTC

which year exactly ?

because end of 2023 is now close.

If you feel a post has answered your question, please click on " Best Answer ".
SimonePradolini
ST Technical Moderator
Nov 29, 2023 11:55 AM UTC

We're testing now the package. If no issues will come up in the next days, the package should be online in wk51 '23, else in wk3 '24.

 

Best regards

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Visitor II
Nov 29, 2023 12:17 PM UTC

@SimonePradolini 

The wk51'23 is making my project in risk but better than nothing. 

If it's wk3'24, my project will be completely dead. So, please, please provide it wk51 and early is even better. Thank a lot in advance.

ST Employee
Nov 30, 2023 9:38 AM UTC

The DLL included in the UltrasoundFFT project within X-CUBE-MEMSMIC1 is not corrupted as stated in the compiler message, it is simply meant to be compiled with GCC and not MSVC.

When you load the project, if you select MinGW 32-bit as a compiler, you are able to compile everything without any issue.

Visitor II
Dec 1, 2023 9:53 AM UTC

@Davide G Yes, it works. Thank you, Thank you so much for help.