Skip to main content
DJadc.1
Associate II
Mar 25, 2022 9:33 AM UTC
Question

Trouble to implement Azure example for board B-L4S5I-IOT01A to Stm32CubeIDE

Hi,

Recently I have been trying to implement an example from ST where data is sent telemetry to Azure. The problem is that Stm32CubeIDE did not generate Netxduo / addons / azure_iot. I am trying to manually add this folder but there are a lot of errors regarding includes and in the example I do not see these folders and files, although in some files they have #include "nx_azure_iot_json_reader.h" which is part of azure-sdk-for-c. If you have any ideas where you need to select somewhere in Stm32CubeIDE to generate this file, please give me advice.

Link to example: https://github.com/azure-rtos/getting-started/tree/master/STMicroelectronics/B-L4S5I-IOT01A

Stm32CubeIDE version: 1.8

This topic has been closed for replies.

19 replies

Haithem Rahmani
ST Employee
Mar 26, 2022 1:26 PM UTC

Hi @DJadc.1​ 

could you please share the errors you are getting?

regards

Haithem.

DJadc.1
DJadc.1Author
Associate II
Mar 26, 2022 2:07 PM UTC

0693W00000LvqLYQAZ.pngFor now i have problem with these two file which have:

#include <curl/curl.h>

#include <windows.h>

I don't know why Stm32CubeIDE don't generate azure_iot folder so i have to put it manually. if you have idea where i need to select in Stm32CubeIDE option which allows to generate this folder

@Haithem Rahmani​ 

Haithem Rahmani
ST Employee
Mar 26, 2022 2:25 PM UTC

Have a look at this microsoft package it offers applications the azure_iot for B-L4S5I-IOT01A board.

there your can notice the relevant files imported from the sdk_iot.

hope this helps.

DJadc.1
DJadc.1Author
Associate II
Mar 26, 2022 2:36 PM UTC

@Haithem Rahmani​ 

Oo thanks it will be very helpful, tonight i will try something with this. if it will work properly i will annouce here

DJadc.1
DJadc.1Author
Associate II
Mar 26, 2022 7:17 PM UTC

Okey so it works but works at AzureIoTHub and i want to work it at AzureIoTCentral. I was trying to put datas from AzureIoTCentral but i don't see host name or ENDPOINT (serviceOperationsHostName {Your DPS name}.azure-devices-provisioning.net). Do you have any idea where i can get it?

@Haithem Rahmani​ 

DJadc.1
DJadc.1Author
Associate II
Mar 26, 2022 9:33 PM UTC

Okey so i fix it. if you want send datas to Azure IoT Central you need to activate DPS and fill #define ENDPOINT "global.azure-devices-provisioning.net" and the rest of the data is self-explanatory

This will be work :D

DJadc.1
DJadc.1Author
Associate II
Mar 29, 2022 12:11 AM UTC

@Haithem Rahmani​ 

I got a problem with porting example project to my new. This problem is related with SysTick because program is going to infinite loop when i click step over before func HAL_Delay(value); I was trying to change SysTick timer to another timer but it given worse result. If you have some free time and you can help me with that i will really thankful. Below is screen with where is the problem and i attach zip file with my project.

0693W00000Lw3U4QAJ.png

Haithem Rahmani
ST Employee
Mar 29, 2022 6:53 AM UTC

there are 3 common use cases for this problem

  • the SysTick is being used by both RTOS & HAL IP driver

keep the Systick for the RTOS and select another timer for the HAL (TIM6)

  • The HAL_Delay is called in an interrupt context (WIFI_REST_MODULE() )

The HAL_Delay won't run because the SYSTICK_PRIORITY is usally less than the current interrupt no preamption is possible.

you'll need to call the "WIFI_REST_MODULE" outside the interrupt mode.

  • The WIFI_REST_MODULE() is called while the RTOS is not yet initialized

the THREADX is disabling the interrupts while initializing thus you'll need to call the WIFI_REST_MODULE either before the tx_kernel_start() or

in a thread entry function.

hope this helps.

regards

Haithem.

DJadc.1
DJadc.1Author
Associate II
Mar 29, 2022 11:22 AM UTC

@Haithem Rahmani​ 

Okey so i set SysTick on TIM6 and i tried wifi init before tx_kernel_start() and in thread entry function and this is not work. Do you have any ideas why? or Can you possibly debug the project which i sent in prev message?

0693W00000Lw7YoQAJ.png0693W00000Lw7Z3QAJ.png

Haithem Rahmani
ST Employee
Mar 29, 2022 9:18 PM UTC

Hi,

you are initializing several IPs alongside the WiFi Module, are you sure that there isn't any PIN conflict in your settings?

regards

haithem.

DJadc.1
DJadc.1Author
Associate II
Mar 30, 2022 7:47 PM UTC

.