Skip to main content
Associate
Oct 8, 2026 1:53 PM UTC
Question

STM32U5G9J-DK2 application example "Fx_NoR_Write_Read_File" is still not working

In the topic “STM32U5G9J-DK2 application example \"Fx_NoR_Write_Read_File\" is not working” there is a problem described which I fear still is present today. The ticket mentioned there is 180260, can someone please check if the patch mentioned is available by now?

Thanks.

2 replies

ST Technical Moderator
Oct 9, 2026 1:43 PM UTC

Hello ​@Mike_SSS 

The issue related to the ticked 180260 has been released in the STM32CubeU5 V1.7.0

The ticket 180260 is related to the post below:

STM32U5G9J-DK2 application example "Fx_NoR_Write_Read_File" is not working | Community

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Mike_SSSAuthor
Associate
Oct 15, 2026 8:12 AM UTC

Wha I did to get to the problem:

  • load the example project into STMCubeU5(1.9.0)
  • generate code for the STM32CubeIDE
  • build that project
  • load project onto the recently aquired -dk2 board
  • debug the situation untill I came to the exact same problem at exactly the same place as the issue referenced

Could you please verify at your end that the project is running successfully on the DK2 board and the issue is indeed fixed?