Skip to main content
digidhamu
Associate III
Apr 28, 2024 1:32 PM UTC
Solved

STM32U5G9J-DK2 application example "Fx_NoR_Write_Read_File" is not working

I encountered an issue with the "Fx_NoR_Write_Read_File" application example. Upon running the application, it consistently triggers an error that redirects control flow to the Error_Handler() function within the app_filex.c file.

Note that STM32U5G9J-DK2 is a brand new board.

Application example location:

../STM32Cube/Repository/STM32Cube_FW_U5_V1.5.0/Projects/STM32U5G9J-DK2/Applications/FileX/Fx_NoR_Write_Read_File

Entering to app_filex.c function Error_Handler() here.

 nor_xspi_status = fx_media_format(&nor_xspi_flash_disk, // nor_xspi_flash_disk pointer
 fx_stm32_levelx_nor_driver, // Driver entry
 (VOID *)NOR_DEFAULT_DRIVER, // Device info pointer
 (UCHAR *) fx_nor_xspi_media_memory, // Media buffer pointer
 sizeof(fx_nor_xspi_media_memory), // Media buffer size
 FX_NOR_XSPI_VOLUME_NAME, // Volume Name
 FX_NOR_XSPI_NUMBER_OF_FATS, // Number of FATs
 32, // Directory Entries
 FX_NOR_XSPI_HIDDEN_SECTORS, // Hidden sectors
 LX_STM32_XSPI_FLASH_SIZE / FX_NOR_XSPI_SECTOR_SIZE, // Total sectors
 FX_NOR_XSPI_SECTOR_SIZE, // Sector size
 8, // Sectors per cluster
 1, // Heads
 1); // Sectors per track

 /* Check the format nor_xspi_status */
 if (nor_xspi_status != FX_SUCCESS)
 {
 Error_Handler();
 }

Could you please help me on this

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
Apr 29, 2024 10:03 AM UTC

Hello,

thank you for your report,

I reproduced the problem and entered a ticket.

Edit: Internal ticket number: 180260.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

4 replies

Mike_ST
Mike_STBest answer
ST Technical Moderator
Apr 29, 2024 10:03 AM UTC

Hello,

thank you for your report,

I reproduced the problem and entered a ticket.

Edit: Internal ticket number: 180260.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
digidhamu
digidhamuAuthor
Associate III
Apr 29, 2024 1:56 PM UTC

Thanks @Mike_ST and will wait for your update.

Visitor II
Jun 11, 2024 10:09 PM UTC

I also had the same issue, wish I saw this post a few days ago. I was trying to port the solution over to my custom project with unexplained errors. Then I ran the example application and also had this same issue. @Mike_ST do you know when an update will be coming?

Thanks.