Skip to main content
Associate II
Sep 12, 2025 8:52 AM UTC
Question

STM32u5 ADC not reading properly a single channel

Split from this thread.

I did and it is all the same.

Here is an example when I measure on port PB1 the voltage from VREF divided by 3 (2.5V/3 = 0,833..V).

Voltage checked with multimeter.

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
uint16_t AD_RES = 0;
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC1_Init(void);
static void MX_ICACHE_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ADC1_Init();
 MX_ICACHE_Init();
 /* USER CODE BEGIN 2 */
 HAL_PWREx_EnableVddA();
 //HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 HAL_ADC_Start(&hadc1);
	 HAL_ADC_PollForConversion(&hadc1, 100);
	 AD_RES = HAL_ADC_GetValue(&hadc1);
	 HAL_Delay(1);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_MSIK;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.MSIKClockRange = RCC_MSIKRANGE_2;
 RCC_OscInitStruct.MSIKState = RCC_MSIK_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
 RCC_OscInitStruct.PLL.PLLM = 2;
 RCC_OscInitStruct.PLL.PLLN = 18;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC1 Initialization Function
 * None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV8;
 hadc1.Init.Resolution = ADC_RESOLUTION_14B;
 hadc1.Init.GainCompensation = 0;
 hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief ICACHE Initialization Function
 * None
 * @retval None
 */
static void MX_ICACHE_Init(void)
{

 /* USER CODE BEGIN ICACHE_Init 0 */

 /* USER CODE END ICACHE_Init 0 */

 /* USER CODE BEGIN ICACHE_Init 1 */

 /* USER CODE END ICACHE_Init 1 */

 /** Enable instruction cache in 1-way (direct mapped cache)
 */
 if (HAL_ICACHE_ConfigAssociativityMode(ICACHE_1WAY) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_ICACHE_Enable() != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ICACHE_Init 2 */

 /* USER CODE END ICACHE_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

I think it can't be done in the simpler way. 

According to the settings 

  • 2.5V Vref
  • VPB1 = 0,833V

I should get something around 5458cnts (14bit) or 1365cnts (12bit).

Unfortunately I am getting something around 0x14.

aristot_0-1757667115573.png

 

 

I am wondering if the fact that I am doing measurements in debug mode may have impact.

I used to work with other controllers and it was working well but maybe sTM32s can't do it.

 

 

This topic has been closed for replies.

9 replies

aristotAuthor
Associate II
Sep 12, 2025 1:06 PM UTC

To exclude issues with debug mode I build release with the measurements being send out through the UART3.

Still measurements as before are incorrect.

No idea how to make ADC work properly.

aristot_0-1757682400165.png

 

aristotAuthor
Associate II
Sep 12, 2025 1:53 PM UTC

I did monitoring of 2 out of 4 channels using MCUmonitor and did notice that the reading periodicaly drop to 0.

Is that something else is trying access the same ports as ADC inputs. How to check it?

aristot_0-1757685198648.png

 

TDK
Sep 12, 2025 2:03 PM UTC

Looks like a code bug or readout issue more than anything else.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TDK
Sep 12, 2025 1:55 PM UTC

The ADC needs calibrated after startup before it can be used.

You don't seem to be initializing any channel to be sampled. Can you include the IOC?

"If you feel a post has answered your question, please click ""Accept as Solution""."
aristotAuthor
Associate II
Sep 12, 2025 3:46 PM UTC

OK I solved the problem for the single channel reading.

It seems there is serious bug in the CubeMx. It doesn't generate complete initialisation code.

In my case the mux selection was missing. So I was basically measuring nothing as none of the physical input was connected to SAR input. 

mƎALLEm
ST Technical Moderator
Sep 12, 2025 4:10 PM UTC

@aristot wrote:

It seems there is serious bug in the CubeMx. It doesn't generate complete initialisation code.

In my case the mux selection was missing. So I was basically measuring nothing as none of the physical input was connected to SAR input. 


Hello,

In that case please open a new thread in STM32CubeMx forum board, So CubeMx team will manage it and please share your solution in this thread and accept it as solution to make it visible for others.

Thank you.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
aristotAuthor
Associate II
Sep 13, 2025 5:02 PM UTC

I am sorry, I was wrong again.

In fact when I did not select the option "Enable Regular convertions" (Cube allows for that) it doesn't generate the Rank for single input.

aristot_0-1757782242784.png

As result there was no input selected in PCSEL register and so I measured nothing getting the values around 15cnts. When I corrected it I started to get different values like 208cnts. Still doesn't make any sense assuming there is 0,833..V at the input. Then I accidentaly change the input setting from single-ended to differential. I got then value around 5440cnts. By accident it was really close to the value I had at the input so I assumed I solved problem somehow.

But it was false assupmtion. No matter which of theese three cases I have they have one thing in common.

They don't change at all no matter what I have at the input. So even if I am change this 0,833V to anything else from the range the readings ale all time tha same with little noise ( +/- 5counst or so)

For some reason it looks like my ADC is totaly disconnected from the input.

I tried to swtich to other inputs as well but no change.

 

TDK
Sep 16, 2025 12:32 PM UTC

> For some reason it looks like my ADC is totaly disconnected from the input.

In the picture you posted above, you were getting readings but about 50% of them went to 0. I wouldn't say the ADC looks disconnected. Are you now seeing different behavior?

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Technical Moderator
Sep 16, 2025 10:07 AM UTC

Hello @aristot 

Did you check the ADC examples provided in STM32Cube firmware U5 ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om