Skip to main content
Linas L
Senior
Feb 17, 2025 8:42 AM UTC
Question

STM32N6 CSI Interface with Raspberry Pi Camera Module 2 NoIR

Hello,

Is there any chance ST could provide examples or guidance on interfacing a CSI (MIPI) camera with Raspberry Pi Camera Module 2 NoIR cameras?

From my initial research, it seems the CSI connector uses the same pin layout as Raspberry Pi cameras. However, available examples are quite limited, making it challenging to implement this on my own — especially compared to the simplicity of working with DCMI.

Any documentation, sample code, or community insights would be greatly appreciated!

Thank you.

LinasL_0-1739781451488.png

LinasL_1-1739781596267.png

With best regards,
Linas

17 replies

ST Technical Moderator
Feb 17, 2025 2:10 PM UTC

Hello,

The N6 STM32Cube firmware ships with some examples for the N6 discovery kit that might be of interest.

If you have CubeMX 6.13 and have downloaded the firmware for N6 through there i would suggest looking at that. They can be found at:

C:\Users\<your_user>\STM32Cube\Repository\STM32Cube_FW_N6_V1.0.0\Projects\STM32N6570-DK\Applications\DCMIPP

There are two examples, one for continous view and one for snapshots.

Let me know if that is of any use :)

Linas L
Linas LAuthor
Senior
Feb 18, 2025 8:10 AM UTC

I will try to do that, but problem is I can't do any measurements on data signals, so everything needs to be made in blind. Also where are tons of registers that I need to get access ( to explanation of registers and also set everything correctly, so it would work with STM32N6) , and it is hard for individuals to get this information.

I would think this example would be quite useful for all STM32 community.

ST Technical Moderator
Feb 18, 2025 3:33 PM UTC

Hello,

If you can get a data sheet for the sensor on your camera, there may be values provided for the parameters set in the two example projects. you may also be able to figure out how it is configured and used in Linux and convert that to something that works in the example projects.

ST supplies a camera module with the STM32N6570-DK, I don't think there are plans to provide examples for other camera hardware at this time.

EmbeddedChris
Associate II
Sep 8, 2025 7:13 AM UTC

Hello Linas, 

Did you manage to get this working? I'm also trying to get the Raspberry pi Camera working and having the same issue as you. 

Thanks,

Chris

Linas L
Linas LAuthor
Senior
Sep 17, 2025 8:35 AM UTC

Camera that was I interested to work with STM32N6 was not good match for my application, so I dropped this testing.

I am having hard time with STM32N6 even for debugging, it's just so many extra steps and so far i was unable to blink even LED... I am using EWARM as my IDE

EmbeddedChris
Associate II
Sep 23, 2025 8:07 AM UTC

Hi Linas,

Thanks for your reply. I was able to get the camera working with help from ST https://community.st.com/t5/stm32-mcus-products/stm32n6-imx219/m-p/839041#M285731

The STM32N6 is difficult to work with. I switched from EWARM to CubeIDE but still encountered issues. I did find that not all of the internal memories are enabled after reset, which caused numerous programming and debugging issues. Could you be having the same issue?

ST Technical Moderator
Sep 23, 2025 11:39 AM UTC

The STM32N6 is difficult to work with. I switched from EWARM to CubeIDE but still encountered issues. I did find that not all of the internal memories are enabled after reset, which caused numerous programming and debugging issues. Could you be having the same issue?


I believe that is a clocking issue - try setting your external memories to be clocked from HCLK in CubeMX.

There is a guide to setting up debugging i CubeIDE here: How to debug STM32N6 using STM32CubeIDE - STMicroelectronics Community

Linas L
Linas LAuthor
Senior
Sep 23, 2025 4:00 PM UTC

It would be nice is EWARM example is made, since for this day, I was unable to make let toggle...

EmbeddedChris
Associate II
Sep 24, 2025 7:10 AM UTC

Sorry to say but I was unable to debug anything on EWARM despite updating to the latest version of the IDE and installing the N6 patches. Not even the ST examples would work because it didn't like the external loader. The examples seemed to run okay in CubeIDE though.  

ST Technical Moderator
Sep 25, 2025 7:12 AM UTC

Did you follow the guide in the link I posted earlier?

In any case, the problem with trying to break at main() is that the symbols for the application are not loaded when you start the debugging session from the FSBL. I'm not sure when that happens when using the guide I posted earlier, but you should be able to break in the debugger just before entering the application (i think he sets it up to do that in the guide), and then add your break point in main. Otherwise, you can step into the application, an then set your breakpoint at that point.

You can also try downloading TouchGFX and looking at the board setup for N6 there - it incorporates some of the same concepts as described in the guide, but implemented differently. You should be able to remove TouchGFX from the project using CubeMX (and removing some references in the .extsettings file) if you're not interested in using that.

Associate III
Oct 3, 2025 3:09 AM UTC

Hi @Linas L  Can you please help me understand how you connected Raspberry Pi Camera Module 2 NoIR to STM32N6 eval board, as Raspberry Pi Camera Module 2 NoIR has 15pin but STM32N6 board has 22pin ? 

 

 

Saeid_0-1759460869640.png

Saeid_1-1759460869836.png

 

Linas L
Linas LAuthor
Senior
Oct 3, 2025 4:18 AM UTC

Simple.

Pi5 has special cable for this. You can buy it in mouser/digikey. Since just like pi zero, pi5 use same 0.5mm pitch connector on pcb

Associate III
Oct 3, 2025 5:12 AM UTC

Wow nice! Thanks Linas for sharing this.

can you please share Digiky/Mouser link that I can buy ? 
In this cable, the VCC from pin# 15  has been mapped to pin#22 ,right?

Associate
Sep 15, 2026 9:38 AM UTC

​@Saeid are you able to make it work. I have used FFC cable i can detect camera but in DCMIPP/NPU hardware territory. 
If you have solved it could be please share how did you do it?