Skip to main content
Associate II
Aug 7, 2025 3:26 PM UTC
Question

STM32H7S78-DK USB hangs in init

Hello, I am trying to utilize the USB peripheral in STM32cubeIDE with the STM32H7S78-DK. It hangs forever in MX_USB_INIT on a function USB CORE RESET. With FS and HS this same issue seems to be happening. Pictures show config in the GUI and the aforementioned function.

This topic has been closed for replies.

9 replies

AScha.3
Super User
Aug 7, 2025 7:43 PM UTC

Hi,

So you have device USB enabled,

For... What kind of device?

I don't see any...

What you want?

 

If you feel a post has answered your question, please click on " Best Answer ".
mtc65536Author
Associate II
Aug 7, 2025 7:51 PM UTC

Hello,
I wish to use it as communication device class, or human interface device class. At the moment I have been configuring it as communication device class in the GUI.

AScha.3
Super User
Aug 7, 2025 8:04 PM UTC

So you set CDC/VCP in Cube?

Int for USB enabled in NVIC settings?

Then it should work, out of the box.

But I don't yet try it on H7S7, only H743, H7A3...

So no guarantees....

If you feel a post has answered your question, please click on " Best Answer ".
Associate III
Aug 12, 2025 10:01 AM UTC

Hello @mtc65536 

I have the same problem, the application hangs at USB CORE RESET,  and I don't understand why. Did you solve the problem?

Associate III
Aug 12, 2025 10:59 AM UTC