Skip to main content
Associate III
Dec 23, 2025 5:27 PM UTC
Solved

STM32H7S3L8 Dual ADC Multichannel + DMA

Hello guys,

for my bachelors project I have decided to build an embedded signal monitoring and classification tool, based on the STM32H7S3L8 Nucleo dev board (NUCLEO H7S3L8). I want to use all  14 available channels of the 2 adcs (technically each ADC has 14, but then pin assignments are shared, which is not beneficial) and i want to let the ADCs stream the data via HPDMA in the SDRAM. Unfortioutly I came across many problems with the configuration and programming, especially with clock configuration of the ADC+DMA in the scanning mode. 

Do some of you already have a working solution to the DMA placement in SDRAM (0x300000 32kB I believe) and with working ADCs you would like to share. 

Also, do you enable callbacks in that case?

Usually I would share my config and code and ask for help to the specific problem, but as I am not at home and already lost my mind with this ******* DMA I might try it that way.

Thanks so much and happy holidays !

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 24, 2025 9:47 AM UTC

Hello,


@htxy wrote:

Do some of you already have a working solution to the DMA placement in SDRAM (0x300000 32kB I believe) and with working ADCs you would like to share. 


First, I don't know from which document you get that information: SDRAM has that address range (0x300000)?

SDRAM memory range is located at that memory range according to the RM0477 / Figure 3. Memory map:

mALLEm_0-1766569373104.png

 

Second, start to configure SDRAM: start by this knowledge base article: How to set up the FMC peripheral to interface with the SDRAM IS42S16800F-6BLI from ISSI

Then do read/write access to the SDRAM. If all are ok start doing a DMA transfers from/to SDRAM and ensure you configure the correct MPU config for data coherency between CPU/DMA:

- AN4839 "Level 1 cache on STM32F7 Series and STM32H7 Series"

- AN4838  "Introduction to memory protection unit management on STM32 MCUs"

Then move on with ADC transfers to SDRAM.

Hope that helps at some points.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 24, 2025 9:47 AM UTC

Hello,


@htxy wrote:

Do some of you already have a working solution to the DMA placement in SDRAM (0x300000 32kB I believe) and with working ADCs you would like to share. 


First, I don't know from which document you get that information: SDRAM has that address range (0x300000)?

SDRAM memory range is located at that memory range according to the RM0477 / Figure 3. Memory map:

mALLEm_0-1766569373104.png

 

Second, start to configure SDRAM: start by this knowledge base article: How to set up the FMC peripheral to interface with the SDRAM IS42S16800F-6BLI from ISSI

Then do read/write access to the SDRAM. If all are ok start doing a DMA transfers from/to SDRAM and ensure you configure the correct MPU config for data coherency between CPU/DMA:

- AN4839 "Level 1 cache on STM32F7 Series and STM32H7 Series"

- AN4838  "Introduction to memory protection unit management on STM32 MCUs"

Then move on with ADC transfers to SDRAM.

Hope that helps at some points.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.