Skip to main content
Associate III
May 7, 2026
Question

STM32H757 SDMMC + FATFS consistently returns FR_NOT_READY

Hello,

I’m working on an STM32H757 (Cortex-M7 core, dual-core system) using SDMMC1 + FATFS (CubeMX-generated stack) and I consistently hit a blocking issue:

  1.  Core issue

f_mount() always returns:

FR_NOT_READY

or the execution breaks inside Error_Handler() depending on build/debug timing.

 Hardware / system context

  • MCU: STM32H757 (Cortex-M7, DCache enabled)

  • SD interface: SDMMC1, 4-bit mode

  • DMA: enabled (CubeMX SDMMC DMA configuration)

  • External subsystem: Riverdi TFT display 12.1 inches (LTDC active)

  • FATFS: CubeMX middleware (generic SD diskio template)

  • No RTOS


 Software architecture

  • STM32CubeIDE latest

  • HAL SDMMC driver (CubeMX generated)

  • FATFS with sd_diskio.c DMA template

  • BSP layer present (mixed HAL/BSP abstraction)

  • Cache enabled (I/D Cache ON, MPU default CubeMX config)


Observed behavior

During initialization:

  • BSP_SD_Init() returns OK

  • SD card is physically detected

  • HAL_SD_GetCardState() does NOT consistently reach SD_TRANSFER_OK

  • SD_CheckStatusWithTimeout() frequently times out

  • FATFS layer reports:

FR_NOT_READY

Mount never succeeds.


Key observations (important)

  • SDMMC peripheral initializes without error

  • DMA transfer callbacks are triggered inconsistently

  • No explicit DCache maintenance is performed in user code

  • MPU remains CubeMX default (no SD/DMA region tuning)

  • sd_diskio.c is the CubeMX DMA template version (unaltered logic)


 Suspected root causes

At this point I strongly suspect one (or more) of the following:

1. Cache coherency issue (most likely)

No explicit:

  • SCB_CleanDCache_by_Addr

  • SCB_InvalidateDCache_by_Addr

around SDMMC DMA buffers.

Given Cortex-M7 behavior, this alone can fully explain:

  • stuck SD state machine

  • invalid transfer completion flags

  • FATFS seeing STA_NOINIT → FR_NOT_READY


2. MPU configuration not DMA-safe

Default CubeMX MPU configuration appears unchanged.

Risk:

  • SDMMC DMA buffer located in cacheable region

  • or MPU attributes conflicting with DMA access


3. SDMMC HAL/BSP mismatch

CubeMX-generated stack mixes:

  • HAL_SD

  • BSP_SD_*

  • FatFS diskio DMA template

The abstraction layering is inconsistent and may be causing:

  • incorrect card state polling

  • race conditions in BSP_SD_GetCardState()


4. SDMMC clock / init sequencing sensitivity

Even though init returns OK, the card never reliably reaches transfer state under FATFS load.


 Question to ST / senior devs

Is there a known stable reference configuration for STM32H757 SDMMC + FATFS + DMA that actually works under Cortex-M7 cache enabled system?

Specifically:

  • Is DCache maintenance mandatory in sd_diskio.c for H7 family even with BSP DMA template?

  • Should MPU explicitly mark SD DMA buffers as non-cacheable?

  • Is the CubeMX SDMMC DMA template actually valid for H757 or known broken in real-world use cases?

  • Any recommended HAL/BSP layering for stable FATFS on H7?

At this point the behavior looks less like an application bug and more like a system-level coherency issue in the generated stack.


Any concrete working reference or confirmed fix would be appreciated.

Thanks.

2 replies

ST Technical Moderator
May 8, 2026

Hello @Sasa1234 


@Sasa1234 wrote:

Is there a known stable reference configuration for STM32H757 SDMMC + FATFS + DMA that actually works under Cortex-M7 cache enabled system?

 Please refer to the example FatFs_Shared_Device in STM32CubeH7.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Sasa1234Author
Associate III
May 21, 2026

Hello everyone,

I've been working for a couple of days on a project using a Riverdi 12-inch display based on an STM32 MCU (STM32H7 series, to be precise). I modified a single line of code inside fatfs_platform.c (Re: Riverdi 12.1" + TouchGFX 4.25 + FATFS not work... - STMicroelectronics Community) – the low‑level FatFs driver provided by STM32CubeMX – to better adapt it to my SDMMC/SDIO peripheral.when I run this main code 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file fatfs.c
 * @brief Code for fatfs applications
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
#include "fatfs.h"

uint8_t retSD; /* Return value for SD */
char SDPath[4]; /* SD logical drive path */
FATFS SDFatFS; /* File system object for SD logical drive */
FIL SDFile; /* File object for SD */

/* USER CODE BEGIN Variables */



#define LED_OK LED1
#define LED_ERROR LED2
#define APP_OK 0
#define APP_ERROR -1
#define APP_SD_UNPLUGGED -2
#define APP_INIT 1
#define FATFS_MKFS_ALLOWED 1
typedef enum {
 APPLICATION_IDLE = 0,
 APPLICATION_INIT,
 APPLICATION_RUNNING,
 APPLICATION_SD_UNPLUGGED,
}FS_FileOperationsTypeDef;

FS_FileOperationsTypeDef Appli_state_uSD = APPLICATION_IDLE;
uint32_t is_initialized = 0;
int32_t ProcessStatus = 0;
static int32_t FS_FileOperations(void);
static void SD_Init(void);
static uint8_t workBuffer[_MAX_SS]; /* a work buffer for the f_mkfs() */

volatile int32_t process_res = APP_OK;

static int32_t FS_FileOperations(void)
{
 FRESULT res; /* FatFs function common result code */
 uint32_t byteswritten, bytesread; /* File write/read counts */
 uint8_t wtext[] = "This is STM32 working with FatFs and uSD diskio driver"; /* File write buffer */
 uint8_t rtext[100]; /* File read buffer */

 /* Register the file system object to the FatFs module */
 if(f_mount(&SDFatFS, (TCHAR const*)SDPath, 0) == FR_OK)
 {
	 res = f_open(&SDFile, "gennarino.TXT", FA_CREATE_ALWAYS | FA_WRITE);
 /* Create and Open a new text file object with write access */
 if(res == FR_OK)
 {
 /* Write data to the text file */
 res = f_write(&SDFile, wtext, sizeof(wtext), (void *)&byteswritten);

 if((byteswritten > 0) && (res == FR_OK))
 {
 /* Close the open text file */
 f_close(&SDFile);

 /* Open the text file object with read access */
 if(f_open(&SDFile, "M.TXT", FA_READ) == FR_OK)
 {
 /* Read data from the text file */
 res = f_read(&SDFile, rtext, sizeof(rtext), (void *)&bytesread);

 if((bytesread > 0) && (res == FR_OK))
 {
 /* Close the open text file */
 f_close(&SDFile);

 /* Compare read data with the expected data */
 if((bytesread == byteswritten))
 {
 // if(Buffercmp((uint32_t *)rtext, (uint32_t *)wtext, sizeof(rtext)))
 { /* Success of the demo: no error occurrence */
 return 0;
 }
 }
 }
 }
 }
 }
 }
 /* Error */
 return -1;
}
/* USER CODE END Variables */

void MX_FATFS_Init(void)
{
 /*## FatFS: Link the SD driver ###########################*/
 retSD = FATFS_LinkDriver(&SD_Driver, SDPath);

 /* USER CODE BEGIN Init */
 Appli_state_uSD = APPLICATION_INIT;
 /* additional user code for init */
 /* USER CODE END Init */
}

/**
 * @brief Gets Time from RTC
 * @PAram None
 * @retval Time in DWORD
 */
DWORD get_fattime(void)
{
 /* USER CODE BEGIN get_fattime */
 return 0;
 /* USER CODE END get_fattime */
}

/* USER CODE BEGIN Application */
void MX_FATFS_Process(void *argument)
{
 /* USER CODE BEGIN MX_FATFS_Process */
	Start_uSD_Test = 1;
 /* Mass Storage Application State Machine */
 while(1)
 {
	 if(Start_uSD_Test)
	 {
 switch(Appli_state_uSD)
 {
 case APPLICATION_INIT:
 if(BSP_SD_IsDetected() == SD_PRESENT)
 {
 // SD_Init();
#if FATFS_MKFS_ALLOWED
 FRESULT res;

 res = f_mkfs(SDPath, FM_ANY, 0, workBuffer, sizeof(workBuffer));

 if (res != FR_OK)
 {
 process_res = APP_ERROR;
 }
 else
 {
 process_res = APP_INIT;
 Appli_state_uSD = APPLICATION_RUNNING;
 }
#else
 process_res = APP_INIT;
 Appli_state_uSD = APPLICATION_RUNNING;
#endif
 }
 else
 {
 Appli_state_uSD = APPLICATION_SD_UNPLUGGED;

 }

 break;
 case APPLICATION_RUNNING:
 // SD_Init();
 process_res = FS_FileOperations();
 Appli_state_uSD = APPLICATION_IDLE;
 Start_uSD_Test = process_res;
 break;

 case APPLICATION_SD_UNPLUGGED:
 process_res = APP_SD_UNPLUGGED;
 break;

 case APPLICATION_IDLE:
 default:
 break;
 }
 ProcessStatus = process_res;
 }
 osDelay(1000);
 }
 /* USER CODE END MX_FATFS_Process */
}

/**
 * @brief BSP SD Initialization
 * @PAram None
 * @retval None.
 */
static void SD_Init()
{
 if (!is_initialized)
 {
 BSP_SD_Init();

 is_initialized = 1;
 }
}

/* USER CODE END Application */

during debugging the variable res becomes FR_DISK_ERR (generic physical drive error). I cannot figure out why.

Attached is my .ioc configuration file 

:question_mark: Question

Has anyone experienced a similar issue when modifying low‑level FatFs drivers on a Riverdi display?
Could this be related to timing, stack/heap size, DMA configuration, or an incorrect implementation of disk_read() / disk_write()?

Any suggestion or shared experience would be greatly appreciated.

Thank you all in advance!