Skip to main content
avarekeci
Visitor II
September 9, 2019
Question

STM32H743ZI CAN BUS Does Not Work

  • September 9, 2019
  • 2 replies
  • 1117 views

I have two STM32H743ZI NUCLEO Boards and I'm trying to communicate through Can Bus protocol in classic mode. In the H7 example projects, there is not an Can example for STM32H743ZI but I tried to adapt example of STM32H743I-EVAL FDCAN project but I couldn't success. How can I solve this? Anyone has tested can config for this board? By the way, I use STM32CubeMX .

This topic has been closed for replies.

2 replies

KModi.1074
Associate
November 7, 2019

I am facing the same issue. Here is my initialization code.

static void MX_FDCAN1_Init(void)

{

FDCAN_FilterTypeDef sFilterConfig;

 /* USER CODE BEGIN FDCAN1_Init 0 */

 /* USER CODE END FDCAN1_Init 0 */

 /* USER CODE BEGIN FDCAN1_Init 1 */

 /* USER CODE END FDCAN1_Init 1 */

 hfdcan1.Instance = FDCAN1;

 hfdcan1.ttcan = NULL;

 hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;

 hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;

 //hfdcan1.Init.Mode = FDCAN_MODE_BUS_MONITORING;

 //hfdcan1.Init.Mode = FDCAN_MODE_INTERNAL_LOOPBACK;

 //hfdcan1.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK;

 hfdcan1.Init.AutoRetransmission = DISABLE;

 hfdcan1.Init.TransmitPause = DISABLE;

 hfdcan1.Init.ProtocolException = DISABLE;

 hfdcan1.Init.NominalPrescaler = (128);

 hfdcan1.Init.NominalSyncJumpWidth = 2;

 hfdcan1.Init.NominalTimeSeg1 = 16;

 hfdcan1.Init.NominalTimeSeg2 = 8;

 /*

 hfdcan1.Init.DataPrescaler = 1;

 hfdcan1.Init.DataSyncJumpWidth = 1;

 hfdcan1.Init.DataTimeSeg1 = 1;

 hfdcan1.Init.DataTimeSeg2 = 1;

 */

 hfdcan1.Init.MessageRAMOffset = 0;

 hfdcan1.Init.StdFiltersNbr = 0;

 hfdcan1.Init.ExtFiltersNbr = 0;

 hfdcan1.Init.RxFifo0ElmtsNbr = 2;

 hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;

 hfdcan1.Init.RxFifo1ElmtsNbr = 0;

 hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;

 hfdcan1.Init.RxBuffersNbr = 0;

 hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;

 hfdcan1.Init.TxEventsNbr = 0;

 hfdcan1.Init.TxBuffersNbr = 0;

 hfdcan1.Init.TxFifoQueueElmtsNbr = 16;

 hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;

 hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;

 if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)

 {

  Error_Handler();

  HAL_Delay(100);

  HAL_UART_Transmit_IT(&huart2,(uint8_t *)"Init Failed\r\n",13);

 }

 else

 {

  HAL_Delay(100);

  HAL_UART_Transmit_IT(&huart2,(uint8_t *)"Init Success\r\n",14);

 }

 /* Configure Rx filter */

  sFilterConfig.IdType = FDCAN_STANDARD_ID;

  sFilterConfig.FilterIndex = 0;

  sFilterConfig.FilterType = FDCAN_FILTER_MASK;

  sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;

  sFilterConfig.FilterID1 = 0x111;

  //sFilterConfig.FilterID2 = 0x7FF; /* For acceptance, MessageID and FilterID1 must match exactly */

  sFilterConfig.FilterID2 = 0x0;

  HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig);

  /* Configure global filter to reject all non-matching frames */

  //HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_REJECT_REMOTE, FDCAN_REJECT_REMOTE);

  /* Configure Rx FIFO 0 watermark to 2 */

  HAL_FDCAN_ConfigFifoWatermark(&hfdcan1, FDCAN_CFG_RX_FIFO0, 1);

  /* Start the FDCAN module */

     if(HAL_FDCAN_Start(&hfdcan1) != HAL_OK)

     {

       HAL_Delay(100);

       HAL_UART_Transmit_IT(&huart2,(uint8_t *)"Start Failed\r\n",14);

     }

     else

     {

       HAL_Delay(100);

       HAL_UART_Transmit_IT(&huart2,(uint8_t *)"Start Success\r\n",15);

     }

  /* Activate Rx FIFO 0 watermark notification */

  HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_WATERMARK | FDCAN_IT_TX_COMPLETE, 0);

  /* Prepare Tx Header */

   TxHeader.Identifier = 0xFF;

   TxHeader.IdType = FDCAN_STANDARD_ID;

   TxHeader.TxFrameType = FDCAN_DATA_FRAME;

   TxHeader.DataLength = FDCAN_DLC_BYTES_1;

   TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;

   TxHeader.BitRateSwitch = FDCAN_BRS_OFF;

   TxHeader.FDFormat = FDCAN_CLASSIC_CAN;

   TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;

   TxHeader.MessageMarker = 0;

 /* USER CODE BEGIN FDCAN1_Init 2 */

 /* USER CODE END FDCAN1_Init 2 */

}

Please let me know if I am doing something wrong.

Tesla DeLorean
Guru
November 7, 2019
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..