cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743ZI CAN not working

KModi.1074
Associate II

I am trying to use the STM32H743I-EVAL FDCAN_Com_IT example code to run CAN on STM32H743ZIT6. I am trying to transmit at regular intervals. When I look the signals on a scope, the TXD goes low for just a bit interval and then remains high. Here is my initialization code.

static void MX_FDCAN1_Init(void)

{

FDCAN_FilterTypeDef sFilterConfig;

 /* USER CODE BEGIN FDCAN1_Init 0 */

 /* USER CODE END FDCAN1_Init 0 */

 /* USER CODE BEGIN FDCAN1_Init 1 */

 /* USER CODE END FDCAN1_Init 1 */

 hfdcan1.Instance = FDCAN1;

 hfdcan1.ttcan = NULL;

 hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;

 hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;

 //hfdcan1.Init.Mode = FDCAN_MODE_BUS_MONITORING;

 //hfdcan1.Init.Mode = FDCAN_MODE_INTERNAL_LOOPBACK;

 //hfdcan1.Init.Mode = FDCAN_MODE_EXTERNAL_LOOPBACK;

 hfdcan1.Init.AutoRetransmission = DISABLE;

 hfdcan1.Init.TransmitPause = DISABLE;

 hfdcan1.Init.ProtocolException = DISABLE;

 hfdcan1.Init.NominalPrescaler = (128);

 hfdcan1.Init.NominalSyncJumpWidth = 2;

 hfdcan1.Init.NominalTimeSeg1 = 16;

 hfdcan1.Init.NominalTimeSeg2 = 8;

 /*

 hfdcan1.Init.DataPrescaler = 1;

 hfdcan1.Init.DataSyncJumpWidth = 1;

 hfdcan1.Init.DataTimeSeg1 = 1;

 hfdcan1.Init.DataTimeSeg2 = 1;

 */

 hfdcan1.Init.MessageRAMOffset = 0;

 hfdcan1.Init.StdFiltersNbr = 0;

 hfdcan1.Init.ExtFiltersNbr = 0;

 hfdcan1.Init.RxFifo0ElmtsNbr = 2;

 hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;

 hfdcan1.Init.RxFifo1ElmtsNbr = 0;

 hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;

 hfdcan1.Init.RxBuffersNbr = 0;

 hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;

 hfdcan1.Init.TxEventsNbr = 0;

 hfdcan1.Init.TxBuffersNbr = 0;

 hfdcan1.Init.TxFifoQueueElmtsNbr = 16;

 hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;

 hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;

 if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)

 {

  Error_Handler();

  HAL_Delay(100);

  HAL_UART_Transmit_IT(&huart2,(uint8_t *)"Init Failed\r\n",13);

 }

 else

 {

  HAL_Delay(100);

  HAL_UART_Transmit_IT(&huart2,(uint8_t *)"Init Success\r\n",14);

 }

 /* Configure Rx filter */

  sFilterConfig.IdType = FDCAN_STANDARD_ID;

  sFilterConfig.FilterIndex = 0;

  sFilterConfig.FilterType = FDCAN_FILTER_MASK;

  sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;

  sFilterConfig.FilterID1 = 0x111;

  //sFilterConfig.FilterID2 = 0x7FF; /* For acceptance, MessageID and FilterID1 must match exactly */

  sFilterConfig.FilterID2 = 0x0;

  HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig);

  /* Configure global filter to reject all non-matching frames */

  //HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_REJECT_REMOTE, FDCAN_REJECT_REMOTE);

  /* Configure Rx FIFO 0 watermark to 2 */

  HAL_FDCAN_ConfigFifoWatermark(&hfdcan1, FDCAN_CFG_RX_FIFO0, 1);

  /* Start the FDCAN module */

     if(HAL_FDCAN_Start(&hfdcan1) != HAL_OK)

     {

       HAL_Delay(100);

       HAL_UART_Transmit_IT(&huart2,(uint8_t *)"Start Failed\r\n",14);

     }

     else

     {

       HAL_Delay(100);

       HAL_UART_Transmit_IT(&huart2,(uint8_t *)"Start Success\r\n",15);

     }

  /* Activate Rx FIFO 0 watermark notification */

  HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_WATERMARK | FDCAN_IT_TX_COMPLETE, 0);

  /* Prepare Tx Header */

   TxHeader.Identifier = 0xFF;

   TxHeader.IdType = FDCAN_STANDARD_ID;

   TxHeader.TxFrameType = FDCAN_DATA_FRAME;

   TxHeader.DataLength = FDCAN_DLC_BYTES_1;

   TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;

   TxHeader.BitRateSwitch = FDCAN_BRS_OFF;

   TxHeader.FDFormat = FDCAN_CLASSIC_CAN;

   TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;

   TxHeader.MessageMarker = 0;

 /* USER CODE BEGIN FDCAN1_Init 2 */

 /* USER CODE END FDCAN1_Init 2 */

}

Please do let me know if I am doing something wrong.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

https://community.st.com/s/question/0D50X0000BJ1WupSQF/stm32h743zi-can-bus-does-not-work

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Richard Li
Senior

Why set this:

"hfdcan1.Init.NominalPrescaler = (128);"

In my mind, the Prescaler never >=32.

Richard

peeyush
Associate

did you get any solution ?

BSpoe.1
Associate III

You should check if the EVAL board has all needed connections to the transceiver / bus. On the STM32H745ZI-Q board there is a solder bridge missing for CAN_TX or CAN_RX line. After soldering the pad my CAN project works! Maybe the H743 Eval board has the same 'problem'...

And why you use such a high prescaler? It's recommended to use the smallest possible prescaler for the CAN peripheral. I think the example project has a prescaler of 1 if you use FDCAN.