Skip to main content
Associate
Apr 11, 2025 7:07 AM UTC
Solved

STM32H743I-EVL example not working with STM32H757I-EVL board

I have purchased STM32H757I-EVL board for working. I have not found SDK for this board. But as one of site suggest downloading STM32CubeH7 package, I did same. In this package I couldn't find example project for STM32H757I-EVL board.
So, I have start working with STM32H743I-EVL example code and compile Thread Creation example. Now I am flashing generated .elf file to STM32H757I-EVL board but this application is not working, and LED is not blinking. I have soldered resistor for LED that is only change on board. I have checked schematic for both board and found it is pin compatible. Now I am stuck to go further. Please anyone found this type of issue or help on this. Meanwhile I will try further and debug issue.
Example code path is STM32CubeH7\Projects\STM32H743I-EVAL\Applications\FreeRTOS\FreeRTOS_ThreadCreation\STM32CubeIDE.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Apr 11, 2025 7:54 AM UTC

Hello @bharatbhardava and welcome to the ST Community

First the STM32H757I-EVL is based on a Dual Core (Cortex-M7 and Cortex-M4) MCU. But the STM32H743I-EVL is based on the Cortex-M7 (one Cortex only). So, For the STM32H757I-EVL, it may have some issues with examples made based on the STM32H743I-EVL. I suggest you use the examples made for the STM32H747I-EVL. The H757I-EVAL is Same as H747I-EVAL but with HASH and CRYP unit.​

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Apr 11, 2025 7:54 AM UTC

Hello @bharatbhardava and welcome to the ST Community

First the STM32H757I-EVL is based on a Dual Core (Cortex-M7 and Cortex-M4) MCU. But the STM32H743I-EVL is based on the Cortex-M7 (one Cortex only). So, For the STM32H757I-EVL, it may have some issues with examples made based on the STM32H743I-EVL. I suggest you use the examples made for the STM32H747I-EVL. The H757I-EVAL is Same as H747I-EVAL but with HASH and CRYP unit.​

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Apr 11, 2025 9:00 AM UTC

Hello,

Example code given for STM32H747I-EVL is working for STM32H757I-EVL. Thank you for help and appreciated for prompt reply.

Andrew Neil
Super User
Apr 11, 2025 9:01 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.